Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Powering a Yun
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 417 subscribers
  • Views 1306 views
  • Users 0 members are here
  • yun
  • ardunio
  • powering
  • question
Related

Powering a Yun

markvenn
markvenn over 11 years ago

Hi all

 

Question for you all regarding the powering of an Arduino Yun. As it is not like the Uno or Mega ADK in that is does not take a range of voltages and seems to be expecting a nice 5V usb supply, if I want to set one up as a standalone bit of kit can I supply power via 1.5V cells 3 x 1.5 = 4.5V? I see that I should be able to power using PoE but I was wondering if I could use it wifi only for some project ideas. I sort of think that 4.5V is not going to be good enough and I don't really want to stick 6V in as this is too much and the web page Arduino - ArduinoBoardYun seems to say that the 5V is the absolute limit. Does anyone have experience with battery powered Yun?

 

Cheers

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 11 years ago +1
    Something like this might work for you: 3A UBEC for Raspberry Pi - Dawn Robotics
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Go for more volts then use an inexpensive and efficient buck convertor to drop the volts to 5V (6 1.5V cells or a pair of LIPO would work ) with little loss of power due to the regulation process, using a LDO linear regulator is also an option but you will waste a significant amount of your available power as heat dissipation in the regulator

     

    My assumption is the 1.%V cells are alkaline, not re-chargeable NIMH as the volts for those re different

     

    Btw, if you use NIMH re-chargeablea, as there nearer 1.2V, not 1.5 you can use four of those to make 4.8V ish, much better to use without a regulator

     

    http://en.wikipedia.org/wiki/Nickel%E2%80%93metal_hydride_battery

     

    hope this helps

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago

    Go for more volts then use an inexpensive and efficient buck convertor to drop the volts to 5V (6 1.5V cells or a pair of LIPO would work ) with little loss of power due to the regulation process, using a LDO linear regulator is also an option but you will waste a significant amount of your available power as heat dissipation in the regulator

     

    My assumption is the 1.%V cells are alkaline, not re-chargeable NIMH as the volts for those re different

     

    Btw, if you use NIMH re-chargeablea, as there nearer 1.2V, not 1.5 you can use four of those to make 4.8V ish, much better to use without a regulator

     

    http://en.wikipedia.org/wiki/Nickel%E2%80%93metal_hydride_battery

     

    hope this helps

     

    Peter