Arduino Forum Contact control with bypass button
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
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 392 subscribers
  • Views 305 views
  • Users 0 members are here
  • arduino_programming_language
Related

Contact control with bypass button

Former Member
Former Member over 10 years ago

I am new to Arduino and would like to make this work but do not know enough about programmingcode to make this work.

Any help would be appreciated.

I have attached a scematic of what I think it should be, but I am not an engineer.

 

Inputs:

 

Relay 1 controlled by outboard source.

 

Relay 2 controlled by outboard source.

 

Push Button 1 ( Toggles LED and Relay 3 )

 

Outputs:

 

Relay 3 ( used to shunt an outboard N.C. contact on another system )

 

LED1

 

Function

 

When RELAY 1 is closed LED turns ON and LED stays ON

 

When RELAY2 is closed LED turns OFF and stays OFF

 

When PUSHBUTTON1 is pressed is will turn OFF LED and turn ON Relay3 and stay ON

 

When PUSHBUTTON is pressed again LED will turn on and RELAY3 will be turned OFF and stay OFF

 

When Relay2 it turns OFF LED and LED stays OFF. Relay3 should also be OFF and stay OFF

 

Basically when I open the access door the doors contact will be bypassed until I push the button again which will unbypass the access doors contact.  Relay2 turns of the LED and Relay3 until it is triggered again by Relay1.

 

Message was edited by: Robert Pfeifer Thanks to all who are helping with this. I have updated my drawing and description of how this should work.

 

Message was edited by: Robert Pfeifer  I have updated the input relay states from two second close to stay closed.

Attachments:
imagecontact_CNTRL_bypass_2-7-14.pdf
  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 10 years ago

    I presume those are the switches at the bottom.  Your uP will have no way to tell which of the two has been depressed.  Otherwise, not too bad for an rl startin' out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 10 years ago

    I presume those are the switches at the bottom.  Your uP will have no way to tell which of the two has been depressed.  Otherwise, not too bad for an rl startin' out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to D_Hersey

    Thanks for your suggestion.

    I have seperated the two and placed them on different inputs.