Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino uno custom board : code not getting uploaded.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 25 replies
  • Subscribers 421 subscribers
  • Views 3792 views
  • Users 0 members are here
  • arduino
Related

Arduino uno custom board : code not getting uploaded.

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I am new to this field, so u guys have to help me with this problem.   I have designed a custom ARDUINO UNO board using Eagle CAD for my project, I haven't changed much in the original arduino design, very little changes where made according to my need. I got the PCB fabricated and the components got  soldered. When i tried to plug the device to PC it got detected and i used FLIP to install the drivers. But the problem lies in uploading the code.when i try to upload a code snippet ( a basic example) , it shows an error like: avrdude:board not in sync . I have tried most of the tutorials given in internet for making the error fine. But nothing helped, so am uploading the design here , U guys please help with some solutions . 

Attachments:
arduino.zip
  • Sign in to reply
  • Cancel
Parents
  • ramyar
    0 ramyar over 11 years ago

    Hi,

    I have tried uploading an irremote program in my freeduino but during uploading process i got the following lines on the screen:

                                                                                                                                                                                                                                                                            

    avrdude: Version 5.11, compiled on Sep  2 2011 at 19:38:36

             Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/

             Copyright (c) 2007-2009 Joerg Wunsch

     

             System wide configuration file is "C:\Program Files (x86)\Arduino\hardware/tools/avr/etc/avrdude.conf"

     

             Using Port                    : \\.\COM3

             Using Programmer              : arduino

             Overriding Baud Rate          : 115200

    avrdude: Send: 0 [30]   [20]

    avrdude: Send: 0 [30]   [20]

    avrdude: Send: 0 [30]   [20]

    avrdude: Recv:

    avrdude: stk500_getsync(): not in sync: resp=0x00

     

    avrdude done.  Thank you.

     

       I tried every possible possible way discussed in many forums,rebooted,installed the drivers again,reset device manager.but the same problem exsists,

    but while updating device manager,i could'nt find arduino.ino file.

    pls anyone suggest  a solution.I am tierd of trying everything.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to ramyar

    Have you ever successfully uploaded any program before this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ramyar
    0 ramyar over 11 years ago in reply to clem57

    Thanks for replying!first I used it with a laptop,it worked well.Now I am using it with my desktop,will there be any problem?  I am using it second time after a month....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to ramyar

    YW. Are you using same Windows on both laptop and desktop? Are you using same USB cable? This message usually says bad communication between your PC and the arduino. Do you see arduino in device manager? In the IDE select port again...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ramyar
    0 ramyar over 11 years ago in reply to clem57

    No,it's not the same.And when I use update driver option,it is recognised as usb device not specifically as arduino r freeduino

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Ramu
    0 Ramu over 11 years ago in reply to ramyar

    As Lab assistant in robotics lab, I have encountered few problems when arduino USB to serial atmel chip got something wrong inside. Do not remember how they were acting. But I have found that sometimes this hapens with older firmware. So I got an Updated firmware (I think somewhere in arduino site) and uploaded using my mkII programmer. then it was ok. If USB to serial chip isn't atmel, but PL232 or something like this, then it may be chinies copy. and for thous new drivers give error "device can't start". then you need to use older drivers. I have pl232 vista (or PL2302). they work when you install them manually and from available drivers list select older one. And sometimes there is windows strange way of understanding serial device as a ball point mouse. It happens when arduino has a code inside wich seas for it to start sending something over serial as soon as arduino gets power. Maybe this is how windows detected Rs232 mouse in an old days. image and some board types have more then one type of chip. be shure to select correct one.

    I hope something got you on track.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Ramu
    0 Ramu over 11 years ago in reply to ramyar

    As Lab assistant in robotics lab, I have encountered few problems when arduino USB to serial atmel chip got something wrong inside. Do not remember how they were acting. But I have found that sometimes this hapens with older firmware. So I got an Updated firmware (I think somewhere in arduino site) and uploaded using my mkII programmer. then it was ok. If USB to serial chip isn't atmel, but PL232 or something like this, then it may be chinies copy. and for thous new drivers give error "device can't start". then you need to use older drivers. I have pl232 vista (or PL2302). they work when you install them manually and from available drivers list select older one. And sometimes there is windows strange way of understanding serial device as a ball point mouse. It happens when arduino has a code inside wich seas for it to start sending something over serial as soon as arduino gets power. Maybe this is how windows detected Rs232 mouse in an old days. image and some board types have more then one type of chip. be shure to select correct one.

    I hope something got you on track.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 11 years ago in reply to Ramu

    Ramu

    Lets start with the basics.

    ENSURE you don't have anything plugged into Arduino Digital pins D0 or D1.

     

    If you follow the troubleshooting guide here, you can then refer to where it stops.

    Arduino - Troubleshooting

    In particular you need to select the correct board as it sets up the communication spedd relative to the bootloader you installed into the 328 chip.

     

    Windows does play funny with the UNO so check under the Device Manager when the board is plugged in.

    Don't be afraid to delete the driver and start again.

     

    Various antivirus software can interfere during the install process.

     

    I'm curious about the answer to this question.

    First, have you loaded the boot loader in the Arduino chip.

    Your answer

    Thanks Dave,

    I have used atmega 16 u2 , and uploaded the firmware.

     

    As far as I'm aware it is not possible to upload the bootloader using the serial connection on its own inot a raw chip.

    So my question is ...

         Did you purchase a 328 chip with the bootloader already installed.?

         If so,  which version of bootloader is installed.?

     

    re this

    it is recognised as usb device not specifically as arduino r freeduino

    The 16u2 will have a PID and UID programmed in which is licenced to arduino ... hence yours will be a standard USB connection.

     

    For comparison the official UNO circuit is here.

    http://arduino.cc/en/uploads/Main/arduino-uno-schematic.pdf

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Ramu
    0 Ramu over 11 years ago in reply to mcb1

    As I understand You use atmega16u2 for USB to Serial conversion. and uploaded firmware to it. So I hope it is the correct one but for your Atmega328 you need bootloader too. And that you can only do with programmer mkII or usbasp. In some cases you can use other arduino as a programmer.

    Its all here: https://learn.sparkfun.com/tutorials/installing-an-arduino-bootloader/connecting-the-programmer

    And like I sead. I do not know why, but sometimes atmega16u2 fails to program the main chip. I had this problem with 2 or 3 adruino boards (we have about 14 of them) over 23 or 3 years of using them. so this may be tour problem.

    And like mcb1 seas, be shure not to connect anything to serial pins when programming it.

     

    By the way. is your main chip showing any signs of life? can you use some programmer and read its signature and memory? Maybe it is dead?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ramyar
    0 ramyar over 11 years ago in reply to mcb1

    The main chip is Atmega8a,it has a built in boot program.To burn it,which board has to be connected to the pc.I am just starting to learn programming with arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Ramu
    0 Ramu over 11 years ago in reply to ramyar

    Ok. in few projects we were using atmega8a with bootlouder ment for it. But it had problem if you were selecting board with atmega8. Sometimes it uploaded the code, sometimes it didn't. So one of the students were selecting arduino UNO (if I remember corectly). Then it was uploading. just this way before uplouding you have to see how much memory and ram the code is taking compiled. and see if it will fit. because atmega8a memory is smaller then atmega328p. Or you just can test with blink code. I was surprised that it worked, because there may be diference in addresing. but it worked. so if erything fales you can try it. But I advise you to rewrite firmware to atmega16u3 and atmega8 with programmer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ramyar
    0 ramyar over 11 years ago in reply to Ramu

    Ok,i will try rewriting with programmer and let u known the result.But even the blink program had the same error...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to ramyar

    We seem  to have two different people having issues with Arduino.

     

    Dhananjayan Selvaraj has a 328 on a custom board and hasn;t replied about the bootloader.

     

    Meanwhile

    Ramya A has a problem with an Atmega8 but not supporting info.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ramyar
    0 ramyar over 11 years ago in reply to mcb1

    I tried the blink program in my friends Laptop and it worked.there is a problem with my CPU.thanks all.... 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to ramyar

    YW Ramya...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to mcb1

    Hi all,

    Sorry for the delay . I am having the latest bootloader In 328.

     

    Thanks & regards ,

    Dhananjayan,

    Zybots

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago in reply to e14 Contributor

    dhananjayan100

    In your original post you'r not showing the error you get.

    I suspect it is avrdude: stk500_getsync(): not in sync: resp=0x00

    This indicates the IDE is not able to talk with the bootloader in the 328 Chip.

     

    I incorrectly tagged the wrong person when asking these questions.

    Please go back to this

    http://www.element14.com/community/message/141676/l/re-arduino-uno-custom-board-code-not-getting-uploaded#141676

    and advice on the answers.

     

     

    I'm happy to try to hlep, but I do require the information, in order to suggest a proper solution.

     

    Thanks Mark