Arduino Forum HELP PLEASE with sketch
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
  • State Not Answered
  • Replies 10 replies
  • Subscribers 404 subscribers
  • Views 739 views
  • Users 0 members are here
  • help
  • sketch
Related

HELP PLEASE with sketch

Former Member
Former Member over 10 years ago

I have a short 15 line sketch for a UNO.  It is to read a ultra sonic sensor and out put the results to the computer.  I will not compile. and has an error that I cannot find.  Is there some one who would be willing to help me find the problem.

 

If I knew how I would put it on the forum here if that would be OK.  I am not sure how to do that though.

  • Sign in to reply
  • Cancel

Top Replies

  • dtsartsanis
    dtsartsanis over 10 years ago in reply to Former Member +2
    Your code miss the void setup section put Serial.begin (9600); pinMode(trigPin, OUTPUT); pinMode(echoPin, INPUT); to void setup section and i believe will work
  • dmaruska
    dmaruska over 10 years ago in reply to clem57 +1
    I just did a search and found the HC-SR04 which used the Trig and Echo pins. I presume this is the sensor that he is using.
Parents
  • clem57
    0 clem57 over 10 years ago

    Ok, please do the following to get more information:

    Under FILE, click on PREFERENCES.

    Check the boxes for verbose for both COMPILE and UPLOAD.

    Run the sketches and you should see a lot of information. Cpature this and post so we can see what may have happened.

    Thank you,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    Ok, please do the following to get more information:

    Under FILE, click on PREFERENCES.

    Check the boxes for verbose for both COMPILE and UPLOAD.

    Run the sketches and you should see a lot of information. Cpature this and post so we can see what may have happened.

    Thank you,

    Clem