Arduino Forum Where should I go to learn about steppers motors?
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
  • State Verified Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 402 subscribers
  • Views 777 views
  • Users 0 members are here
  • information
  • motors
  • learning
Related

Where should I go to learn about steppers motors?

lokkytron
lokkytron over 10 years ago

Well, I am trying to make a choice about dc motor with variable speed or step by step motor with microsteps driver to control the mechanism that I explained here

 

What i need to know is: Is there any resource in this site or another where i can start to learn about dc motors?

 

I am making random readings after many searches in google... but i don't know enough about these motors to get usefull information.

 

Thank you.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +4 suggested
    You could read a bit about a few different types of motors here: http://www.element14.com/community/community/applications/industrial-automation/blog/2015/02/14/motors--pm-dc-bldc-servo-stepper-moving…
  • neilk
    neilk over 10 years ago +2 suggested
    Hi lokkytron you could also have a quick look here: http://www.element14.com/community/people/neilk/blog/2015/01/24/arduino-controlling-stepper-motor-28byj-48-with-accelstepper-library and perhaps here…
  • peterjcs23
    peterjcs23 over 10 years ago +1
    Sounds like you need to control speed and position, in which case the stepper motor is a straightforward solution if you are not looking for very high speed or very high torque. If you use a dc motor you…
Parents
  • peterjcs23
    0 peterjcs23 over 10 years ago

    Sounds like you need to control speed and position, in which case the stepper motor is a straightforward solution if you are not looking for very high speed or very high torque. If you use a dc motor you will have to add a speed and position feedback device such as an encoder and a more complex controller that a stepper controller. Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • peterjcs23
    0 peterjcs23 over 10 years ago

    Sounds like you need to control speed and position, in which case the stepper motor is a straightforward solution if you are not looking for very high speed or very high torque. If you use a dc motor you will have to add a speed and position feedback device such as an encoder and a more complex controller that a stepper controller. Peter