Hello ALL
I'm a new arduino user and at my school I have to create a User interface using GUI Matlab wich will control arduino code load on the robot with 20 servos
I'll apreciate your help
Thanks in advance.
Hello ALL
I'm a new arduino user and at my school I have to create a User interface using GUI Matlab wich will control arduino code load on the robot with 20 servos
I'll apreciate your help
Thanks in advance.
HI and thanks so so much to answer me
I hope this is the beginning of the response for the question. I'm working
on a project which have to establish communication between a human robot
based on arduino board and a pc and smartphone. First with the computer
using serial then after with a smartphone using adaFruit Bluetooth module
for arduino and an android application which I have to develop using
eclipse or any.
I have written a arduino code on my best as a arduino-servo beginner for a
humanoid robot. I have to control the robot by a matlab user interface GUI
as said. The fact is communication between the arduino mega ADK for android
and the matlab GUI using serial. I connect using fopen(my_serial) but I
don't know how to send commands from UI edit text, pushbutton and how to
select the port from a popup menu. Soon I will post the code.
I will really appreciate your help
Thanks in advance
Le 13 mars 2015 17:03, "gadget.iom" <messages@element14.com> a écrit :
image: element14
<http://www.element14.com?CMP=e14notificationemail_header> How to
control Arduino from Matlab GUI(with, popup menu selecting Serial Com,
pbtton to send data, edit txt to input char to send) created by Paul
Ellison <http://www.element14.com/community/people/gadget.iom> in
Arduino - View the full discussion
First of all, Hello to everyone, because this is my first post here in this community and I hope I am not doing it wrong.
I do have a good step by step video tutorial for your problem, where you can see the whole procedure of making that communication between the Arduino and Matlab via GUI. You can find that from my website at the following link:
http://howtomechatronics.com/tutorials/arduino/matlab-gui/
I hope this is helpful to you.
Dejan Nedelkovski