Arduino Forum Components needed for a barebones Arduino
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
  • State Not Answered
  • Replies 9 replies
  • Subscribers 405 subscribers
  • Views 655 views
  • Users 0 members are here
  • atmega328
  • microcontroller
  • arduino
Related

Components needed for a barebones Arduino

Former Member
Former Member over 10 years ago

Is there anything other than the crystal and the microcontroller that is necessary for this? I want to get as little as possible, as this is going somewhere and staying there, and doesn't need any shields or accessories. And also, if I wanted to program it just once, is there a way to ghetto-rig it up to a serial port with jumper wires? Thank You!

  • Sign in to reply
  • Cancel

Top Replies

  • 4ringfan
    4ringfan over 10 years ago in reply to Former Member +4
    Maybe I'm not following this. I'm not sure I understand the need to re-invent the wheel. If you are doing this as a DIY to prove to yourself that you can make a controller from ground up complete with…
  • mcb1
    mcb1 over 10 years ago +1
    Paul has given you some good advise .. and some searching on google will also find plenty ... http://cdn.shopify.com/s/files/1/0038/9582/files/RBBB_Instructions_06.pdf?1260749296 You don't need the resonator…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +1
    Other than the 8MHZ default clock. I believe they don't recommend the internal RC clock for serial due to instability...some even complain about the resonators...not that I've had a problem with those…
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    2 20pF capacitors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to gadget.iom

    OK.  Do you know if I could connect the rx/tx/whatever else I need to connect directly to the serial port?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to Former Member

    Not entirely sure what you mean there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to Former Member

    Not entirely sure what you mean there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to gadget.iom

    Well,  is there any way to program it without an external serial to USB converter?