Arduino Forum Powering the Yun from batteries?
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
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 401 subscribers
  • Views 675 views
  • Users 0 members are here
  • battery
  • lipo
  • arduino_yun
Related

Powering the Yun from batteries?

Workshopshed
Workshopshed over 10 years ago

Any recommendations for powering the Arduino Yun from batteries, I'm looking at the following with an 850mAh battery. I'm not planning on having the Yun turned on all of the time. Any hints and tips?

 

http://www.adafruit.com/product/1944

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago +2
    How about a USB battery charger for the Yun? Works for me. Clem
  • shabaz
    shabaz over 10 years ago +1 suggested
    Hi Andy! One option might be the TI BOOSTXL-BATTPACK which has a 1200mAH battery with it, and has 5V output (and 3.3V optional from memory, using a jumper) so perfect for Yun - as long as you're willing…
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi Andy!

     

    One option might be the TI BOOSTXL-BATTPACK which has a 1200mAH battery with it, and has 5V output (and 3.3V optional from memory, using a jumper) so perfect for Yun - as long as you're willing to use jumper cables to connect them up (since the TI BoosterPack form-factor is not the same as the Arduino shield form-factor).

    I've used the BOOSTXL-BATTPACK with a Raspberry Pi too - works nicely. For that I made myself a little BoosterPack-to-RaspberryPi adapter - see photo below. The file for it is here Temperature Measurement for Lab and Science Projects .

    Unfortunately the BOOSTXL-BATTPACK is 'Awaiting Delivery' on the UK Farnell site currently.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    Hi Andy!

     

    One option might be the TI BOOSTXL-BATTPACK which has a 1200mAH battery with it, and has 5V output (and 3.3V optional from memory, using a jumper) so perfect for Yun - as long as you're willing to use jumper cables to connect them up (since the TI BoosterPack form-factor is not the same as the Arduino shield form-factor).

    I've used the BOOSTXL-BATTPACK with a Raspberry Pi too - works nicely. For that I made myself a little BoosterPack-to-RaspberryPi adapter - see photo below. The file for it is here Temperature Measurement for Lab and Science Projects .

    Unfortunately the BOOSTXL-BATTPACK is 'Awaiting Delivery' on the UK Farnell site currently.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer