Arduino Forum how to attach crystal?
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
  • State Not Answered
  • Replies 19 replies
  • Subscribers 396 subscribers
  • Views 1498 views
  • Users 0 members are here
  • crystal
  • oscillators
  • avr
  • atmega328p
Related

how to attach crystal?

rishi2628
rishi2628 over 10 years ago

i am making a custom board using atmega328p. i am programming the chip using a arduino uno board which works fine but when i attach the microcontroller to the development board, the delay function doesn't seem to work. I think there is a problem with the oscillator. I have simply connected a crystal at xtal pins. Is this the correct way??

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +4
    Something like this... Google "arduino bare bones"
  • mcb1
    mcb1 over 10 years ago in reply to clem57 +3
    clem57 I see to recall we had a very similar discussion not that long ago. ... The Bare Bones project tend to use a resonator, although they talk about a xtal and neglect to say you need the capcitors…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to clem57 +3
    I tend to prefer a real xtal and a couple of caps, this gives a much more precise loop time. Either will work without issue and the cost is still measured in Pennies or Cents If your making thousands then…
Parents
  • rishi2628
    0 rishi2628 over 10 years ago

    ok now i have connected the capacitors along with the oscillator. Still the servo is not working. The code, servo, the soldering connections and the microcontroller are fine, i have checked it all, any suggestions what could be wrong??...................And FYI.............i am programming the atmega on a breadboard without an oscillator and then attaching it to my custom board with the oscillator...........does this cause any problem??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fvan
    0 fvan over 10 years ago in reply to rishi2628

    Just to clarify, the chip has been flashed with the arduino bootloader as well, right ?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rishi2628
    0 rishi2628 over 10 years ago in reply to fvan

    No.........i didn't do that...............let me try that out

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to rishi2628

    rishi2628

         Did you ever finish this build?

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago in reply to rishi2628

    rishi2628

         Did you ever finish this build?

    Clem