Arduino Forum <STX> <ETX> character in Serial Arduino Communication
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 391 subscribers
  • Views 3423 views
  • Users 0 members are here
  • ttl
  • ascii
  • serial
  • etx
  • stx
  • arduino
  • module
Related

<STX> <ETX> character in Serial Arduino Communication

Former Member
Former Member over 10 years ago

Hi to everyone,

 

I'm implementing a serial communication between Arduino Uno and a Non Invasive Blood Pressure Model (NIBScan NIBP OEM module). This module has a RS232 port and I've used a RS232 to TTL converter to wire the module to Arduino.

I must send serial commands to the Module this way:

      <STX>01;;D7<EXT>    => Start measuring

      <STX>18;;DF<EXT>  => Read status from slave.

 

The problem is that I don't know how to correctly send the "<STX>" (0x02)  and "<ETX>" (0x03) chars. I've tried this way:

     blood_pressure_board.print("\u000218;;DF\u0003");

    blood_pressure_board.print("<STX>18;;DF<ETX>");

but it doesn't work.

 

Besides, after booting, the module  has to send a message like this:

    <STX>S1;A0;C00;M00;P135345234;R087;T6890;;D9<ETX><CR>

but what I get into serial monitor of Arduino (setting 4800 baud rate how indicated into the guide) is:

Ë–X`1ƒ¶  fÌ;Mƒ¶µeË–µkÖ¬egÔ-k¶   È�  Û  Í´`Ã�9  Ö˜°jÌ�Á¶  3Ì�Mƒ¶ZgË–-k  Ë–X`˜;ÁMÁk˵j£    9Ë6¬˜°˜;ƒ¶ 3Ì�MÁ¶ YË–-«Ö¬Ù3Ë–íF    dÈ ;  fÚ°á

 

What am I getting wrong?

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1
    Try Serial.write(0x02);
  • clem57
    clem57 over 10 years ago +1
    void WriteDummyWeatherData(){ #define STX Serial.print(STX); Serial.print( " 11 06 2013 12:00=11.78" ); Serial.print(RS); Serial.print( " 11 06 2013 23:00=8.9" ); Serial.print(RS); Serial.print( " 11 07…
  • gadget.iom
    0 gadget.iom over 10 years ago

    Try

    Serial.write(0x02);

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago

    void WriteDummyWeatherData(){

    #define STX

      Serial.print(STX);

      Serial.print("11 06 2013 12:00=11.78");

      Serial.print(RS);

      Serial.print("11 06 2013 23:00=8.9");

      Serial.print(RS);

      Serial.print("11 07 2013 06:00=4.54");

      Serial.print(RS);

      Serial.print("11 07 2013 12:00=15.3");

      Serial.print(RS);

      Serial.print("11 07 2013 23:00=10.3");

      Serial.print(RS);

      Serial.print("11 21 2013 06:00=-2.33");

      Serial.print(ETX);

    }    replace blood_pressure_board for serial.

     

    From Arduino, C#, and Serial Interface - CodeProject

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alpierce
    0 alpierce over 10 years ago

    Have you tried different baud rate settings on the Arduino when you boot the module? They may have changed the rate from 4800 and the documentation does not reflect that.

    Try other rates( 2400, 9600, etc) and see if any of them produce correct output from the module.