Arduino Forum <STX> <ETX> character in Serial Arduino Communication
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 391 subscribers
  • Views 3425 views
  • Users 0 members are here
  • ttl
  • ascii
  • serial
  • etx
  • stx
  • arduino
  • module
Related

<STX> <ETX> character in Serial Arduino Communication

Former Member
Former Member over 10 years ago

Hi to everyone,

 

I'm implementing a serial communication between Arduino Uno and a Non Invasive Blood Pressure Model (NIBScan NIBP OEM module). This module has a RS232 port and I've used a RS232 to TTL converter to wire the module to Arduino.

I must send serial commands to the Module this way:

      <STX>01;;D7<EXT>    => Start measuring

      <STX>18;;DF<EXT>  => Read status from slave.

 

The problem is that I don't know how to correctly send the "<STX>" (0x02)  and "<ETX>" (0x03) chars. I've tried this way:

     blood_pressure_board.print("\u000218;;DF\u0003");

    blood_pressure_board.print("<STX>18;;DF<ETX>");

but it doesn't work.

 

Besides, after booting, the module  has to send a message like this:

    <STX>S1;A0;C00;M00;P135345234;R087;T6890;;D9<ETX><CR>

but what I get into serial monitor of Arduino (setting 4800 baud rate how indicated into the guide) is:

Ë–X`1ƒ¶  fÌ;Mƒ¶µeË–µkÖ¬egÔ-k¶   È�  Û  Í´`Ã�9  Ö˜°jÌ�Á¶  3Ì�Mƒ¶ZgË–-k  Ë–X`˜;ÁMÁk˵j£    9Ë6¬˜°˜;ƒ¶ 3Ì�MÁ¶ YË–-«Ö¬Ù3Ë–íF    dÈ ;  fÚ°á

 

What am I getting wrong?

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +1
    Try Serial.write(0x02);
  • clem57
    clem57 over 10 years ago +1
    void WriteDummyWeatherData(){ #define STX Serial.print(STX); Serial.print( " 11 06 2013 12:00=11.78" ); Serial.print(RS); Serial.print( " 11 06 2013 23:00=8.9" ); Serial.print(RS); Serial.print( " 11 07…
Parents
  • clem57
    0 clem57 over 10 years ago

    void WriteDummyWeatherData(){

    #define STX

      Serial.print(STX);

      Serial.print("11 06 2013 12:00=11.78");

      Serial.print(RS);

      Serial.print("11 06 2013 23:00=8.9");

      Serial.print(RS);

      Serial.print("11 07 2013 06:00=4.54");

      Serial.print(RS);

      Serial.print("11 07 2013 12:00=15.3");

      Serial.print(RS);

      Serial.print("11 07 2013 23:00=10.3");

      Serial.print(RS);

      Serial.print("11 21 2013 06:00=-2.33");

      Serial.print(ETX);

    }    replace blood_pressure_board for serial.

     

    From Arduino, C#, and Serial Interface - CodeProject

     

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    void WriteDummyWeatherData(){

    #define STX

      Serial.print(STX);

      Serial.print("11 06 2013 12:00=11.78");

      Serial.print(RS);

      Serial.print("11 06 2013 23:00=8.9");

      Serial.print(RS);

      Serial.print("11 07 2013 06:00=4.54");

      Serial.print(RS);

      Serial.print("11 07 2013 12:00=15.3");

      Serial.print(RS);

      Serial.print("11 07 2013 23:00=10.3");

      Serial.print(RS);

      Serial.print("11 21 2013 06:00=-2.33");

      Serial.print(ETX);

    }    replace blood_pressure_board for serial.

     

    From Arduino, C#, and Serial Interface - CodeProject

     

    Clem