Arduino Forum Arduino and Bluetooth
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
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 390 subscribers
  • Views 1022 views
  • Users 0 members are here
  • mit_appinventor
  • hc06
  • appinventor
  • bluetooth®
  • arduino
Related

Arduino and Bluetooth

Former Member
Former Member over 10 years ago

I am working with the arduino uno and an HC-06 bluetooth module. My project is for my job and in the end will control the processes of a laser cutting head. basically we have an app that is the "control panel" and controls the arduino. the arduino then controls a PLC which then is sent elsewhere to sensors and the laser. I have the basics done I think but I am stuck trying to figure out how to make the arduino read if there is an error in the system and show a notice message on the app. Also in the app there is a numbers only text box that will be used to manually send measurments to tell the laser where to be. I have no idea how i would write that in arduino. Any help is useful. Here is my code so far...

 

 

int x0 = 13;

int x1 = 12;

int x2 = 11;

int x3 = 10;

int x4 = 9;

int y5 = A0;

 

 

void setup()

{

  Serial.begin(9600);

  pinMode(x0, OUTPUT);

  pinMode(x1, OUTPUT);

  pinMode(x2, OUTPUT);

  pinMode(x3, OUTPUT);

  pinMode(x4, OUTPUT);

  digitalWrite(x0, LOW);

  digitalWrite(x1, LOW);

  digitalWrite(x2, LOW);

  digitalWrite(x3, LOW);

  digitalWrite(x4, LOW);

}

 

 

 

 

 

 

void loop()

{

  delay(100);

  String t;

  while(Serial.available()) {

    t += (char)Serial.read();

  }

 

 

  if(t.length()){

     if(t == "pp on") {

       digitalWrite(x2, HIGH);

       digitalWrite(x0,LOW);

       digitalWrite(x1,LOW);

       digitalWrite(x3, LOW);

       digitalWrite(x4, LOW);

       }

     else if (t == "pp off") {

       digitalWrite(x2, LOW);

      }

    if(t == "auto on") {

      digitalWrite(x0, HIGH);

      digitalWrite(x1,LOW);

      digitalWrite(x2, LOW);

      digitalWrite(x3, LOW);

      digitalWrite(x4, LOW);

    }

    else if (t == "auto off") {

      digitalWrite(x0, LOW);

    }

      if(t == "man on") {

        digitalWrite(x1, HIGH);

        digitalWrite(x0, LOW);

        digitalWrite(x2, LOW);

      }

      else if (t == "man off") {

        digitalWrite(x1, LOW);

      }

      if (t == "up on"){

        digitalWrite(x3, HIGH);

        digitalWrite(x1,HIGH);

        digitalWrite(x0, LOW);

        digitalWrite(x2, LOW);

      }

      else if(t == "up off"){

        digitalWrite(x3, LOW);

        digitalWrite(x1, LOW);

      }

      if (t == "down on"){

        digitalWrite(x4, HIGH);

        digitalWrite(x1, HIGH);

        digitalWrite(x0, LOW);

        digitalWrite(x2, LOW);

      }

      else if(t == "down off"){

        digitalWrite(x4, LOW);

        digitalWrite(x1, LOW);

      }

  }

}

 

If anyone has any segestions on how to make my code i have already better or more simple let me know as well.

 

the app is through MIT app inventor 2 if anyone can help on that end it would be much appreciated. heres a screen shot of what it looks like for visual use...

 

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago in reply to neilk +3
    Cool. Found a few deleted comments appearing in my inbox feed. So many in fact that I ordered a couple of rolls of this:
  • Former Member
    Former Member over 10 years ago in reply to neilk +2
    The arduino code responds based off of the text that is sent from the app. Here is the block code i have so far for the basic funtions of the app. All i need to do now is be able to recieve some sort of…
  • gadget.iom
    gadget.iom over 10 years ago +1 suggested
    Is there a digital out (Y) terminal on the PLC that is/could be for an error signal? If so, you could use a digitalread statement to get that status, and a serial.print to send that to your Bluetooth module…
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    Is there a digital out (Y) terminal on the PLC that is/could be for an error signal?

     

    If so, you could use a digitalread statement to get that status, and a serial.print to send that to your Bluetooth module.

     

    Paul.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 10 years ago

    Is there a digital out (Y) terminal on the PLC that is/could be for an error signal?

     

    If so, you could use a digitalread statement to get that status, and a serial.print to send that to your Bluetooth module.

     

    Paul.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer