Arduino Forum How to Sequentially Activate Pins while Reading from a Sensor ?
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
  • State Not Answered
  • Replies 8 replies
  • Subscribers 392 subscribers
  • Views 561 views
  • Users 0 members are here
Related

How to Sequentially Activate Pins while Reading from a Sensor ?

aureta
aureta over 10 years ago

Hi, I am starting with Arduino and I am in need of some help. I am trying to sequentially activate 5 pins. I need each pin to be active for 20 seconds in a PWM manner. During their active period I want an arduino sensor to constantly read out the signals emmited by each pin effector. So far I have no problems with the PWM or sensing module code. However I am not able to find how to correctly sequentially activate the pins. I used millis(), etc, but so far I was able to only activate / read the signals from the first pin effector. The sketch doesn´t proceed to the 2nd --- pins. I really very much appreciate your help ....

  • Sign in to reply
  • Cancel

Top Replies

  • dtsartsanis
    dtsartsanis over 10 years ago +1
    If you post your code someone will help you
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to aureta +1
    Hello, your mistake is in the use of millis() With this function you get the number of milliseconds occured from the last power-on of the microcontroller . So you should not put while(millis()<5000) because…
Parents
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hello Alejandro,

     

    please post your code or at least your idea of code architecture. Anyway the better solution I see is to use a timer interrupt or a bare interrupt but in this case you have a pin locked by the interrupt trigger. Take in account that using this tecnique you can't use the delay() or millis() count anymore. In many cases I have used millis() that is efficient as it will work in a very similar way as software interrupt. Without your code I think it is really impossible to give you a more detailed advice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hello Alejandro,

     

    please post your code or at least your idea of code architecture. Anyway the better solution I see is to use a timer interrupt or a bare interrupt but in this case you have a pin locked by the interrupt trigger. Take in account that using this tecnique you can't use the delay() or millis() count anymore. In many cases I have used millis() that is efficient as it will work in a very similar way as software interrupt. Without your code I think it is really impossible to give you a more detailed advice.