Arduino Forum pls how do i go about communicating with 2 arduinos with the use of the tx/rx pin.
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
  • State Not Answered
  • Replies 17 replies
  • Subscribers 403 subscribers
  • Views 1747 views
  • Users 0 members are here
Related

pls how do i go about communicating with 2 arduinos with the use of the tx/rx pin.

Former Member
Former Member over 10 years ago

i have codes for pulse sensor, temp sensor, GPS  and i need the readings from the sensors and gps to be sent to the other arduino's LCD. i just dont know how to go about doing it and i was wondering if there is someone that could help guide me.

 

//sender

int inpin=A0;

int TEMP=0;

int heartratepin=A1;

int difference;

int newHeartReading = 0;

int lastHeartReading = 0;

int measurements[5] = {0,0,0,0,0};

int historySize = 5;

int recenttotal = 0;

int Index = 0;

boolean highChange = false;

int minimumdifference = 2;

int num[5];

int average=0;

 

 

// Heart rate timing

long lastHeartbeatTime = 0;

long debounceDelay = 150;       // the debounce time; increase if the output flickers

int currentHeartrate = 0;

int lastHeartrate = 0;

//Heart rate LED

//int ledState = LOW;

//long ledOnMillis = 0;

//long ledOnInterval = 50;

int slope = ((newHeartReading-lastHeartReading)/(debounceDelay-lastHeartrate));

 

 

 

 

 

 

// Debugging string

String debugOutput = "";

void setup() {

   // start serial port at 9600 bps:

   Serial.begin(9600);

    pinMode(heartratepin,INPUT);

   establishContact();

}

void establishContact() {

while (Serial.available() <= 0) {

      Serial.println("hello");   // send a starting message

      delay(300);

   }

}

void loop() {

   // read analog input, divide by 4 to make the range 0-255:

   int analogValue = analogRead(inpin);

   float millivolts = (analogValue/1024.0)*5000;

   float celsius = millivolts/10-50;

   Serial.println(analogValue);

   Serial.print(celsius);

   Serial.print("c");

   Serial.print((celsius*9)/5+32);

   Serial.print("F");

   newHeartReading = analogRead(heartratepin);

    //calculation

  difference = newHeartReading - lastHeartReading;

  lastHeartReading = newHeartReading;

 

  // Find new recent total

  recenttotal = recenttotal - measurements[Index] + difference;

  // replace indexed recent value

  measurements[Index] = difference;

   //index + 1 index = (index + 1) % historySize;

    for (int i=0; i<5; i=i+1){

               num[i]=0;        

   }

    

              if (Index>=5)

              Index=0;

              //calculating the average

              average=recenttotal/5;

              Serial.println(average);

              delay(10);

  if (recenttotal >= minimumdifference)

  {

    // possible heart rate check timing

    if (millis() - lastHeartbeatTime >= debounceDelay)   // whatever the reading is at, it's been there for longer

    // than the debounce delay, so take it as the actual current state:

 

 

    {

  // Heart rate

// digitalWrite(ledPin, HIGH);

  currentHeartrate = 60000 / (millis() - lastHeartbeatTime);

    lastHeartbeatTime = millis();

   Serial.println(newHeartReading);

      if (currentHeartrate <= 200)// && currentHeartrate > 20)

    { 

                 

                  Serial.print("Heart Rate =" + String(currentHeartrate) + "  ");

                  delay(10);

    }

            if (currentHeartrate <= 39 and currentHeartrate >= 0){

                

                  Serial.print("I Am Sick");

                }

                 delay(10);

          if (currentHeartrate<= 79 and currentHeartrate >= 70){

                

                  Serial.print("Night Mare");

                }

                delay(10);

            if (currentHeartrate <= 69 and currentHeartrate >= 40){

               

                  Serial.print("kid Is At Sleep");

          }

              delay(10);

              if (currentHeartrate <= 99 and currentHeartrate >= 80){

                 

                  Serial.print("Kid Is Resting");

             }

                delay(10);

                if (currentHeartrate <= 119 and currentHeartrate >= 100){

                

                  Serial.print("Kid Is Playing");

               }

             

                  if(currentHeartrate > 120){

                   

                    Serial.print(" The Kid Is Having ");

                    //lcd.setCursor(0,1);

                    //lcd.print(" A Heart Attack");

                }

  

  

 

 

   // print different formats:

   Serial.write(analogValue);  // Print the raw binary value

   Serial.print('\t');             // print a tab

   Serial.write(newHeartReading);  // Print the raw binary value

   Serial.print('\t');             // print a tab

 

}

  }

}

 

 

 

//receiver

#include <SPI.h>

#include <LiquidCrystal.h>

int heartratepin=A1;

int inpin=A0;

LiquidCrystal lcd(30,31,32,33,34,35);

void setup()

{

  lcd.begin(16,2);

  Serial.begin(9600);

}

void loop()

{

  if(Serial.available()>0)

  {

    int inByte=Serial.read();

    int analogValue=analogRead(inpin);

    lcd.print(analogValue);

    lcd.print(",");

   

    int newHeartReading=analogRead(heartratepin);

    lcd.print(newHeartReading);

    lcd.print(",");

   

   

 

 

  }

}

 

i dont know what i am doing wrong

  • Sign in to reply
  • Cancel

Top Replies

  • bobcroft
    bobcroft over 10 years ago in reply to Former Member +2
    Richard, in order to see the Easy Transfer library just Google Arduino Easy Transfer library. There are informative notes and code examples. To answer your other question, yes you can display the data…
  • clem57
    clem57 over 10 years ago +1
    ricardo240 I cannot comment on the sender code since it has many things going on. But here are the things I would do: Make sure the pins are connected as TX to RX on the UART on sender and UART on receiver…
  • clem57
    clem57 over 10 years ago in reply to Former Member +1
    To understand: 1) the sensors are reading fine. 2) The UNO sends on UART to the MEGA UART but does not work. What pins are connected on each to the other? 3) The code you sent looks like snippets especially…
Parents
  • gadget.iom
    0 gadget.iom over 10 years ago

    What model of Arduino are you using?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to gadget.iom

    Am using a uno for the sender and a mega for the receiver

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    On the UNO, can you use the UART and have no debugging code or USB support? Paul raises a valid concern because of limited UART.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Yes, i am using a 9v battery source to power to uno so that i wouldnt have to use the usb support as the powering source

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    The reading is taking place, am just having problems getting it to the mega for it to be displayed on the lcd screen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    To understand:

    1) the sensors are reading fine.

    2) The UNO sends on UART to the MEGA UART but does not work. What pins are connected on each to the other?

    3) The code you sent looks like snippets especially receiver and guessing not complete. Can you attach full sketch from both? If you wish put in private blog between us only.

    4) Does the serial code work on the UNO when sent to USB? If it does that would resolve half the issue.

    5) Did you check anything from my first comment?

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    To understand:

    1) the sensors are reading fine.

    2) The UNO sends on UART to the MEGA UART but does not work. What pins are connected on each to the other?

    3) The code you sent looks like snippets especially receiver and guessing not complete. Can you attach full sketch from both? If you wish put in private blog between us only.

    4) Does the serial code work on the UNO when sent to USB? If it does that would resolve half the issue.

    5) Did you check anything from my first comment?

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    1. yes the sensors are working

    2. yes, i am using on the uno pin 0 and 1 for the tx and rx. on the mega i am using pin 18 and 19 for tx and rx

    3.i will send u the code now

    4.yes it does work with the usb connect it self

    5.yes i did.

     

     

    i started with the temp sensor alone

     

     

    #include <SoftwareSerial.h>

     

     

    //reciever

     

     

    #include <SPI.h>

    #include <LiquidCrystal.h>

    SoftwareSerial mySerial(1,0);

    int inpin=A0;

    LiquidCrystal lcd(30,31,32,33,34,35);

    void setup()

    {

      lcd.begin(16,2);

      Serial.begin(9600);

      //Serial1.begin(9600);

    establishContact();

    }

    void establishContact() {

    while (Serial.available()== 1) {

         // Serial.println("hello");   // send a starting message

          delay(300);

        }

    }

    void loop()

    {

      if(Serial.available()==1)

      {

        int inbyte =Serial.read();

        int sensorValue=analogRead(A0);

        lcd.print(sensorValue);

        lcd.print(",");

       

     

    #include <SoftwareSerial.h>

    int inpin=A0;

    int TEMP=0;

    int sensorValue;

    SoftwareSerial mySerial(18,19);

     

     

    void setup() {

       // start serial port at 9600 bps:

       Serial.begin(9600);

     

       // pinMode(heartratepin,INPUT);

      // establishContact();

    }

    //void establishContact() {

    //while (Serial.available()== 1) {

         // Serial.println("hello");   // send a starting message

       //   delay(300);

      

     

    void loop() {

      if (mySerial.available())

      Serial.write(mySerial.read());

      if (Serial.available())

       int sensorValue = analogRead(inpin);

       float millivolts = (sensorValue/1024.0)*5000;

       float celsius = millivolts/10-50;

       Serial.println(sensorValue);

       Serial.print(celsius);

       Serial.print("c");

       Serial.print((celsius*9)/5+32);

       Serial.print("F");

       // print different formats:

      mySerial.write(sensorValue);  // Print the raw binary value

       Serial.print('\t');             // print a tab

    }

     

       

       

     

     

      }

    }