Arduino Forum Sensor Interference
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
  • State Not Answered
  • Replies 12 replies
  • Subscribers 391 subscribers
  • Views 911 views
  • Users 0 members are here
Related

Sensor Interference

aureta
aureta over 10 years ago

Hi, I am working with TSL235 light to frequency converter sensors using an Arduino MEGA ADK. When working with one sensor at a time there is no problem with sensing. When two sensors are simultaneously connected they interfere with each other. How can i fix this problem ?, I am attaching the code being used for the simultaneous reading of two TSL235 sensors. Regards. Alejandro.

 

 

# define TSL235Two 21 // Out of TSL235 connected to Digital pin 21

# define TSL235One 3 // Out of TSL237 connected to Digital pin 3

 

 

int period = 101; // Miliseconds of each light frecuency measurement

 

 

unsigned long counterTwo = 0; // Counter of measurements during the test

unsigned long counterOne = 0; // Counter of measurements during the test

 

 

unsigned long currentTime = millis();

unsigned long startTime = currentTime;

 

 

volatile long pulsesTwo = 0; // Counter of measurements of the TSL235R

volatile long pulsesOne = 0; // Counter of measurements of the TSL235R

 

 

unsigned long frequencyTwo; // Read the frequency from the digital pin (pulses/second)

unsigned long frequencyOne; // Read the frequency from the digital pin (pulses/second)

 

 

 

 

void setup()

{

 

 

  Serial.begin(115200); // Start and configure the serial port

  attachInterrupt(2, PulseCountTwo, RISING);

  attachInterrupt(1, PulseCountOne, RISING);

  pinMode(TSL235Two, INPUT); // Declare the pin such as an input of data

  pinMode(TSL235One, INPUT); // Declare the pin such as an input of data

  setup_parallax();

}

 

 

void loop()

{

 

 

counterTwo++; // Increase the number of measurement

counterOne++; // Increase the number of measurement

getfrequencyTwo(); // Request to measure the frequency

getfrequencyOne(); // Request to measure the frequency

pulsesTwo = 0; // reset the pulses counter                                      

pulsesOne = 0; // reset the pulses counter

parallax_output();

                  

}

 

 

 

 

void PulseCountTwo()

{

pulsesTwo++;

}

 

 

void PulseCountOne()

{

pulsesOne++;

}

 

 

 

 

void parallax_output()

{

   

    Serial.print("DATA,DATE,TIME,");

    Serial.print(frequencyTwo); Serial.print(","); Serial.println(frequencyOne);

   

}

 

 

void setup_parallax()

{

   Serial.println("LABEL,Date,Time,Frequency Two, Frequency One");

}

 

 

 

 

unsigned long getfrequencyOne ()

{

noInterrupts();

frequencyOne = pulsesOne *1000 / period; // Calculate the frequency (pulses/second)

interrupts();

return (frequencyOne);

}

 

 

 

 

unsigned long getfrequencyTwo ()

{

noInterrupts();

frequencyTwo = pulsesTwo *1000 / period; // Calculate the frequency (pulses/second)

interrupts();

return (frequencyTwo);

}

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    When working with interrupts (more than 1) you need to be very careful to masking them. When one comes in while masked, you will loose it. I see you start the two almost same time. Good chance they will interrupt nearly same time. When you handle one, the other is masked off. I suggest you put a small delay between enabling them.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • aureta
    0 aureta over 10 years ago in reply to clem57

    Hi Clem, where at the code should I do this and how?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to aureta

    Your processor is running at 8 or 16Mhz and these sensors output at 200-300 Hz (250 ave):

     

    void loop()

    {

    counterTwo++; // Increase the number of measurement

    counterOne++; // Increase the number of measurement

    getfrequencyTwo(); // Request to measure the frequency

    delay(.000025);     // delay for measurements between the two for 1/250/16

    getfrequencyOne(); // Request to measure the frequency

    pulsesTwo = 0; // reset the pulses counter                                      

    pulsesOne = 0; // reset the pulses counter

    parallax_output();

    }                 

     

    Try this and let me know. This is an estimate and may need adjusting.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • aureta
    0 aureta over 10 years ago in reply to clem57

    Hi Clem, I did try. there still interference, I include a snapshot of the SM. Under the same light conditions, when the sketch starts there is a high count number from sensor at  timer 2 (read before delay), not the results shown by the other one (right column). After a while I obstruct the sensor plugged at timer 1 without any significant change in the output from either one of these.  I then obstruct the sensor plugged at timer 2, this time the readings from sensor at timer one drops quite dramatically while the reading from the sensor plugged at timer two increases (?¿). I added a final delay at the loop but it didn´t have any effect. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to aureta

    Interesting. Would you like to try changing sensor one to a falling signal and leaving sensor two to a rising signal?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • aureta
    0 aureta over 10 years ago in reply to aureta

    i was trying just that but the behavior is basically the same...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • aureta
    0 aureta over 10 years ago in reply to aureta

    i was trying just that but the behavior is basically the same...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to aureta

    Need to go back to thinking...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • aureta
    0 aureta over 10 years ago in reply to clem57

    I appreciate very much your help.