Arduino Forum Sensor Interference
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
  • State Not Answered
  • Replies 12 replies
  • Subscribers 391 subscribers
  • Views 922 views
  • Users 0 members are here
Related

Sensor Interference

aureta
aureta over 10 years ago

Hi, I am working with TSL235 light to frequency converter sensors using an Arduino MEGA ADK. When working with one sensor at a time there is no problem with sensing. When two sensors are simultaneously connected they interfere with each other. How can i fix this problem ?, I am attaching the code being used for the simultaneous reading of two TSL235 sensors. Regards. Alejandro.

 

 

# define TSL235Two 21 // Out of TSL235 connected to Digital pin 21

# define TSL235One 3 // Out of TSL237 connected to Digital pin 3

 

 

int period = 101; // Miliseconds of each light frecuency measurement

 

 

unsigned long counterTwo = 0; // Counter of measurements during the test

unsigned long counterOne = 0; // Counter of measurements during the test

 

 

unsigned long currentTime = millis();

unsigned long startTime = currentTime;

 

 

volatile long pulsesTwo = 0; // Counter of measurements of the TSL235R

volatile long pulsesOne = 0; // Counter of measurements of the TSL235R

 

 

unsigned long frequencyTwo; // Read the frequency from the digital pin (pulses/second)

unsigned long frequencyOne; // Read the frequency from the digital pin (pulses/second)

 

 

 

 

void setup()

{

 

 

  Serial.begin(115200); // Start and configure the serial port

  attachInterrupt(2, PulseCountTwo, RISING);

  attachInterrupt(1, PulseCountOne, RISING);

  pinMode(TSL235Two, INPUT); // Declare the pin such as an input of data

  pinMode(TSL235One, INPUT); // Declare the pin such as an input of data

  setup_parallax();

}

 

 

void loop()

{

 

 

counterTwo++; // Increase the number of measurement

counterOne++; // Increase the number of measurement

getfrequencyTwo(); // Request to measure the frequency

getfrequencyOne(); // Request to measure the frequency

pulsesTwo = 0; // reset the pulses counter                                      

pulsesOne = 0; // reset the pulses counter

parallax_output();

                  

}

 

 

 

 

void PulseCountTwo()

{

pulsesTwo++;

}

 

 

void PulseCountOne()

{

pulsesOne++;

}

 

 

 

 

void parallax_output()

{

   

    Serial.print("DATA,DATE,TIME,");

    Serial.print(frequencyTwo); Serial.print(","); Serial.println(frequencyOne);

   

}

 

 

void setup_parallax()

{

   Serial.println("LABEL,Date,Time,Frequency Two, Frequency One");

}

 

 

 

 

unsigned long getfrequencyOne ()

{

noInterrupts();

frequencyOne = pulsesOne *1000 / period; // Calculate the frequency (pulses/second)

interrupts();

return (frequencyOne);

}

 

 

 

 

unsigned long getfrequencyTwo ()

{

noInterrupts();

frequencyTwo = pulsesTwo *1000 / period; // Calculate the frequency (pulses/second)

interrupts();

return (frequencyTwo);

}

  • Sign in to reply
  • Cancel
Parents
  • neilk
    0 neilk over 10 years ago

    aureta Hi Alejandro

     

    I've been out of town for a few days, so I've only just looked at this problem again.

     

    I can now see one significant problem with your code - but this probably doesn't affect the interference image

     

    You define:

     

    int period = 101; // Miliseconds of each light frecuency measurement

     

    And then use it to calculate your pulse fequency:

     

    frequencyOne = pulsesOne *1000 / period; // Calculate the frequency (pulses/second)

     

    However, your main program loop runs "free" ie it is not controlled so that it executes:

     

    getfrequencyTwo(); // Request to measure the frequency

    getfrequencyOne(); // Request to measure the frequency

     

    at intervals of "period", ie 101 mS ! This means that your sampling period is actually quite short - basically, the execution time of the loop image

     

    have you looked at this:

     

    http://playground.arduino.cc/Main/TSL235R

     

    This uses a call to the millis() function every time the main loop is executed. This controls the pulse reading period.

     

    Another observation is that perhaps the overall light level to which you are exposing the sensors is too high. The frequencies reported in your post #7 are quite high, considering the short (and unknown) sampling period you are ACTUALLY using.

     

    Hope this helps

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • neilk
    0 neilk over 10 years ago

    aureta Hi Alejandro

     

    I've been out of town for a few days, so I've only just looked at this problem again.

     

    I can now see one significant problem with your code - but this probably doesn't affect the interference image

     

    You define:

     

    int period = 101; // Miliseconds of each light frecuency measurement

     

    And then use it to calculate your pulse fequency:

     

    frequencyOne = pulsesOne *1000 / period; // Calculate the frequency (pulses/second)

     

    However, your main program loop runs "free" ie it is not controlled so that it executes:

     

    getfrequencyTwo(); // Request to measure the frequency

    getfrequencyOne(); // Request to measure the frequency

     

    at intervals of "period", ie 101 mS ! This means that your sampling period is actually quite short - basically, the execution time of the loop image

     

    have you looked at this:

     

    http://playground.arduino.cc/Main/TSL235R

     

    This uses a call to the millis() function every time the main loop is executed. This controls the pulse reading period.

     

    Another observation is that perhaps the overall light level to which you are exposing the sensors is too high. The frequencies reported in your post #7 are quite high, considering the short (and unknown) sampling period you are ACTUALLY using.

     

    Hope this helps

     

    Neil