Arduino Forum Arduino - Two Inputs Using the Keypad.
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
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 403 subscribers
  • Views 1848 views
  • Users 0 members are here
Related

Arduino - Two Inputs Using the Keypad.

Former Member
Former Member over 10 years ago

Hey guys,

i am new to arduino. i am currently working on a small project. basically i am using the 4 x 4 keypad for the input and LCD for display. so once the program runs the user enters two value. so first input is 2 digit input which arduino saves in an array and similarly the second input is a four digit input that is saved into the second array. The program runs successfully and reads the first input correctly though the second input does not work.

 

if (int(key1) != 0 and currentState == 1) {

 

switch (key1) {

case '*':

// sets the first array to zero

currentState = 1;

break;

 

case '#':

//saves the value into the first array

//sets the currentState to 2

currentState = 2;

if (currentState = 2){

switch (key1){

case '*':

//sets the second array to zero

currentState = 2;

break;

case '#':

//saves the value into the second array

currentState = 1;

break;

 

case 'A':

//goes back to the menu

break;

 

default:

currentTValue[0] = currentTValue[1];

currentTValue[1] = key1;

break;

}

}

break;

 

case 'A':

//goes back to the menu

break;

 

default:

currentT2Value[0] = currentT2Value[1];

currentT2Value[1] = currentT2Value[2];

currentT2Value[2] = currentT2Value[3];

currentT2Value[3] = key1;

break;

}

}

}

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +3
    You have the classic beginner mistake of using an assignment where you want to perform a comparison currentState = 2 is an assignment not a compare currentState == 2 is a comparison and will return a true…
  • mcb1
    mcb1 over 10 years ago +1 verified
    if (currentState = 2) needs to be if (currentState == 2) Although I'm unsure why you check when you set it the line above and several lines later. Do you really need line 12 and 13 ? if (int(key1) !…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mcb1 +1
    A very good and valid point Mark, I was not intending to deminish your valued input, just focus on the lesser issue of the use of comparison vs assignment operators to help Terry along. And yes, it is…
Parents
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hello,

     

    despite the = / == check in the if that anyway returns a wrong condition respect what you expect but it is a valid assignation so it is NOT a syntax error, I have pasted your code in the IDE, just to see what are the errors - if any. The problem is that what is really important and is missing in your bunch of code is where and how you declare and initialiases the character arrays.

     

    What sounds strange to me, but it is better if you update the post with the topmost part of the code, at least, is the use of the arrays (I suppose character arrays). Please can you add few more lines of code ?

     

    Last but not least, did you took in account that if key  is a char it is also an integer too ?

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago

    Hello,

     

    despite the = / == check in the if that anyway returns a wrong condition respect what you expect but it is a valid assignation so it is NOT a syntax error, I have pasted your code in the IDE, just to see what are the errors - if any. The problem is that what is really important and is missing in your bunch of code is where and how you declare and initialiases the character arrays.

     

    What sounds strange to me, but it is better if you update the post with the topmost part of the code, at least, is the use of the arrays (I suppose character arrays). Please can you add few more lines of code ?

     

    Last but not least, did you took in account that if key  is a char it is also an integer too ?

     

    Enrico