Arduino Forum problem pairing xbee series 1 by puTTy
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 392 subscribers
  • Views 497 views
  • Users 0 members are here
Related

problem pairing xbee series 1 by puTTy

Former Member
Former Member over 10 years ago

Okay, so i just wanted to pair 2 Xbees modules of Series 1 by using puTTY software.

The commands that i should have used were :

For first xbee

+++                    *wait for an OK*
ATMY1000       *ENTER*
ATDL1001.       *ENTER*
ATID1111         *COMMA*
WR                     *ENTER*

For second xbee

+++                    *wait for an OK*
ATMY1001       *ENTER*
ATDL1000        *ENTER*
ATID1111         *COMMA*
WR                     *ENTER*

By mistake, it wrote :

For first xbee

+++                    *wait for an OK*
ATMY1000       *ENTER*
ATDL1001        *ENTER*
ATID1111         *COMMA*
WR                     *ENTER*

For second xbee

+++                    *wait for an OK*
ATMY1001       *ENTER*
ATDL1000        *ENTER*
ATID1111         *ENTER*

+++                    *wait for an OK*
ATMY1001       *ENTER*
ATDL1000        *ENTER*
ATID1111         *COMMA*
WR                     *ENTER*

I started with +++ again for second xbee 'coz i had to type a *comma* instead of *enter* but i did'nt write that time.

So my question is whether it would work or not. Also, what should i do to re-configure them?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    I checked you are ok so long as you do not WR. The WR commits the values to EEPROM. BTW, you can reconfigure them again if needed.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    Now that i've WR the IDs, can i normally re-configure them? Just by starting with +++ ? Like, if i want to change the IDs, won't i need any command to delete the existing IDs? Or would it just normally overwrite over the existing ones? Would it work fine?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Yes. The WR allows them to remember after a power cut. Otherwise they would forget and revert to the last WR.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Yes. The WR allows them to remember after a power cut. Otherwise they would forget and revert to the last WR.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to clem57

    That was very helpful. Thanks.. Btw what's the use of ATCN command? Isn't it necessary?