Arduino Forum Arduino screen with photoresistor
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 500 views
  • Users 0 members are here
  • screen
  • arduino
  • photoresistor
Related

Arduino screen with photoresistor

pot82es
pot82es over 10 years ago

Hi.

 

Im building a mailbox with a screen that changes the message wheter you have mail or not, but I need some help with my code.

 

This is what I have for the moment, but it doesnt seem to work like I would like it to.

 

 

 

#include <LiquidCrystal.h>

#include <LCDKeypad.h>

 

 

LCDKeypad lcd;

 

 

const int threshold = 100;

const int analogPin = A0;

 

 

 

 

void setup() {

 

  int analogValue = analogRead(analogPin);

 

  if (analogValue > threshold)

  {

  lcd.begin(16, 2);

  lcd.print("text1");

  }

  else

  {

  lcd.begin(16, 2);

  lcd.print("text2");

  }

  }

 

 

void loop() {

}

 

Any help is higly appriciated!

 

Be sure to tell me some suggestons, if I should use a photoresistor or not. image

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago +3 suggested
    I don't have the LCDkeypad.h file so I can't verify this runs/compiles. #include <LiquidCrystal.h> #include <LCDKeypad.h> LCDKeypad lcd; const int threshold = 100; const int analogPin = A0; int analogValue;…
  • clem57
    clem57 over 10 years ago +2 verified
    The code in setup runs just 1 time. The code in loop can run many times, but a delay is wise to not overload the sensor with testing. Clem #include <LiquidCrystal.h> #include <LCDKeypad.h> LCDKeypad lcd;…
Parents
  • clem57
    0 clem57 over 10 years ago

    The code in setup runs just 1 time. The code in loop can run many times, but a delay is wise to not overload the sensor with testing.

    Clem

     

     

    #include <LiquidCrystal.h>

    #include <LCDKeypad.h>

     

     

    LCDKeypad lcd;

     

     

    const int threshold = 100;

    const int analogPin = A0;

     

     

     

     

    void setup() {

     

     

      }

     

     

    void loop() {

    int analogValue = analogRead(analogPin);

     

      if (analogValue > threshold)

      {

      lcd.begin(16, 2);

      lcd.print("text1");

      }

      else

      {

      lcd.begin(16, 2);

      lcd.print("text2");

      }

      Delay(1000); // delay 1 second

    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    The code in setup runs just 1 time. The code in loop can run many times, but a delay is wise to not overload the sensor with testing.

    Clem

     

     

    #include <LiquidCrystal.h>

    #include <LCDKeypad.h>

     

     

    LCDKeypad lcd;

     

     

    const int threshold = 100;

    const int analogPin = A0;

     

     

     

     

    void setup() {

     

     

      }

     

     

    void loop() {

    int analogValue = analogRead(analogPin);

     

      if (analogValue > threshold)

      {

      lcd.begin(16, 2);

      lcd.print("text1");

      }

      else

      {

      lcd.begin(16, 2);

      lcd.print("text2");

      }

      Delay(1000); // delay 1 second

    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • pot82es
    0 pot82es over 10 years ago in reply to clem57

    Thank you! image