Arduino Forum Arduino screen with photoresistor
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
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 403 subscribers
  • Views 500 views
  • Users 0 members are here
  • screen
  • arduino
  • photoresistor
Related

Arduino screen with photoresistor

pot82es
pot82es over 10 years ago

Hi.

 

Im building a mailbox with a screen that changes the message wheter you have mail or not, but I need some help with my code.

 

This is what I have for the moment, but it doesnt seem to work like I would like it to.

 

 

 

#include <LiquidCrystal.h>

#include <LCDKeypad.h>

 

 

LCDKeypad lcd;

 

 

const int threshold = 100;

const int analogPin = A0;

 

 

 

 

void setup() {

 

  int analogValue = analogRead(analogPin);

 

  if (analogValue > threshold)

  {

  lcd.begin(16, 2);

  lcd.print("text1");

  }

  else

  {

  lcd.begin(16, 2);

  lcd.print("text2");

  }

  }

 

 

void loop() {

}

 

Any help is higly appriciated!

 

Be sure to tell me some suggestons, if I should use a photoresistor or not. image

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago +3 suggested
    I don't have the LCDkeypad.h file so I can't verify this runs/compiles. #include <LiquidCrystal.h> #include <LCDKeypad.h> LCDKeypad lcd; const int threshold = 100; const int analogPin = A0; int analogValue;…
  • clem57
    clem57 over 10 years ago +2 verified
    The code in setup runs just 1 time. The code in loop can run many times, but a delay is wise to not overload the sensor with testing. Clem #include <LiquidCrystal.h> #include <LCDKeypad.h> LCDKeypad lcd;…
Parents
  • mcb1
    0 mcb1 over 10 years ago

    I don't have the LCDkeypad.h file so I can't verify this runs/compiles.

     

     

    #include <LiquidCrystal.h>
    #include <LCDKeypad.h>
    
    LCDKeypad lcd;
    
    
    const int threshold = 100;
    const int analogPin = A0;
    int analogValue;
    
    
    
    
    void setup() {
      lcd.begin(16, 2);
    
      }
    
    
    void loop() {
      analogValue = analogRead(analogPin);
      lcd.clear;
    
      if (analogValue > threshold)
      {
         
         lcd.print("text1");
      }
      else
      { 
         lcd.print("text2");
      }
    
    delay(1000);
    }

    As Clem pointed out adding a delay stops it just running flat out.

     

    There are some examples in Arduino and each library often adds some more.

    You will find some in LiquidCrystal which you can adapt ...

     

    Mark

     

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago

    I don't have the LCDkeypad.h file so I can't verify this runs/compiles.

     

     

    #include <LiquidCrystal.h>
    #include <LCDKeypad.h>
    
    LCDKeypad lcd;
    
    
    const int threshold = 100;
    const int analogPin = A0;
    int analogValue;
    
    
    
    
    void setup() {
      lcd.begin(16, 2);
    
      }
    
    
    void loop() {
      analogValue = analogRead(analogPin);
      lcd.clear;
    
      if (analogValue > threshold)
      {
         
         lcd.print("text1");
      }
      else
      { 
         lcd.print("text2");
      }
    
    delay(1000);
    }

    As Clem pointed out adding a delay stops it just running flat out.

     

    There are some examples in Arduino and each library often adds some more.

    You will find some in LiquidCrystal which you can adapt ...

     

    Mark

     

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • pot82es
    0 pot82es over 10 years ago in reply to mcb1

    Thank you! image