Arduino Forum Pololu USB AVR Programmer
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
  • State Verified Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 404 subscribers
  • Views 618 views
  • Users 0 members are here
Related

Pololu USB AVR Programmer

gtrplyer16
gtrplyer16 over 10 years ago

Does anyone know if the above programmer is compatible with windows 8?? I bought some ATMega chips and they weren't the right ones so I was going to buy a programmer to mess around with an program it using AVR studio 6 instead of finding an arduino to use them in.

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 10 years ago in reply to clem57 +3 suggested
    Note: This programmer supports standard in-system programming (ISP), which is also sometimes called in-circuit serial programming (ICSP). It does not support JTAG, DebugWire, or High-Voltage programming…
  • clem57
    clem57 over 10 years ago +2 suggested
    Supported Operating Systems The programmer has been tested under Windows XP, Windows Vista, Windows 7, Windows 8, and Linux from https://www.pololu.com/product/1300 Clem
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +2
    I poersonally have the PGM03A and it works across the board (Its a POLOLU Board also)
Parents
  • gtrplyer16
    0 gtrplyer16 over 10 years ago

    My next question which is sort of pointless but I am new to programming using ISP is that the Pololu can program any of the ATMega chips? I have a ATMega328-PU but needed the ATMega328P-PU I believe the first PN is the correct one which I ordered. So I'm just curious as to making sure I'm not buying an AVR ISP Programmer that can not program this chip. So to restate my question: Does the Pololu AVR ISP able to program all the ATMega chips or only specific ones?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gtrplyer16

    This device (And the same as the one I have) will work with most of the Atmel AVR micro-controllers, this is detailed here https://www.pololu.com/product/1300

     

    I have used it with many ATMEGA328 variety chips and ATMEGA2560, U16/U32s, ATTINY84/85 etc with no issues. Basically any ATMEL chip that supports the ISP programming interface (Which is pretty much all of the AVR range, I'm not aware of any that don't have this)

     

    If my response is correct / helpful than please mark as such, it helps me get more badges image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gtrplyer16

    This device (And the same as the one I have) will work with most of the Atmel AVR micro-controllers, this is detailed here https://www.pololu.com/product/1300

     

    I have used it with many ATMEGA328 variety chips and ATMEGA2560, U16/U32s, ATTINY84/85 etc with no issues. Basically any ATMEL chip that supports the ISP programming interface (Which is pretty much all of the AVR range, I'm not aware of any that don't have this)

     

    If my response is correct / helpful than please mark as such, it helps me get more badges image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • gtrplyer16
    0 gtrplyer16 over 10 years ago in reply to Robert Peter Oakes

    Thank you so much for all your help yesterday and today the information you presented was very useful!