Arduino Forum What is the problem?
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
  • State Verified Answer
  • Replies 33 replies
  • Answers 3 answers
  • Subscribers 394 subscribers
  • Views 2144 views
  • Users 0 members are here
  • flickering
Related

What is the problem?

rishi2628
rishi2628 over 10 years ago

I have made the following circuit, can anyone please tell me why the seven segments are flickering. I have used multiplexing, don't tell me it is because of that. I have tried it prototyping on an arduino uno and it worked perfectly.SO its not because of the multiplexing!! and its not the code. I think something is interfering or resetting the microcontroller because it does not store the values on the seven segments.The motors on the right are not connected. Any clue what is wrong?

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago in reply to rishi2628 +2
    RIshi, mcb1 told that there is a power problem NOT because the 7805 is a crap component but because, with a reasonable difficult we are trying to decode your info and seems that your schematic has issues…
  • mcb1
    mcb1 over 10 years ago in reply to balearicdynamics +2
    rishi2628 The syntax highlighting that Enrico is referring to is a little hidden. It's a shame there isn't a simple icon, but we struggled to get it added, so it's better than nothing. past you code, then…
  • clem57
    clem57 over 10 years ago +2
    Why do you automatically discount multiplexing? Just because it worked one place does not mean it works in ALL places... You could have affected other wires while hooking up from the old Uno. Many factors…
Parents
  • Former Member
    0 Former Member over 10 years ago

    Can the atmega actually source/sink the current needed by the display? maybe it's functioning within acceptable parameters to start with but it's probably becoming oversaturated and getting hot resulting in brownouts?

     

    9v batteries don't supply a great amount of power either so definately a nicely sized smoothing cap on the power rails wouldn't go amiss either.

     

    --------------------

    edit:

     

    Do you have a multimeter to check the voltages?

    If you are using a 7805, when they get hot they also start pulsing on and off so just check to make sure it's capable of supplying the current you need and also a temperature check while it's in operation would remove that doubt.

     

    Lucie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to Former Member

    The other link to the previous post suggests that he has a problem whenever the servo(s) are attached.

     

    Unfortunately in the previous post we only got partial information so until we get it all, its hard to say what is happening.

    There are no series resistors on the anode side, but maye they are included in the common.

    Unfortunately he hasn;t answered about the schematic errors, so we really need rishi2628 to read the various ansers and fill in the missing bits.

     

    If he does use a multimeter, it won't show the spikes, but it will show the average voltage.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago in reply to Former Member

    The other link to the previous post suggests that he has a problem whenever the servo(s) are attached.

     

    Unfortunately in the previous post we only got partial information so until we get it all, its hard to say what is happening.

    There are no series resistors on the anode side, but maye they are included in the common.

    Unfortunately he hasn;t answered about the schematic errors, so we really need rishi2628 to read the various ansers and fill in the missing bits.

     

    If he does use a multimeter, it won't show the spikes, but it will show the average voltage.

     

    Mark