Arduino Forum What is the problem?
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
  • State Verified Answer
  • Replies 33 replies
  • Answers 3 answers
  • Subscribers 394 subscribers
  • Views 2144 views
  • Users 0 members are here
  • flickering
Related

What is the problem?

rishi2628
rishi2628 over 10 years ago

I have made the following circuit, can anyone please tell me why the seven segments are flickering. I have used multiplexing, don't tell me it is because of that. I have tried it prototyping on an arduino uno and it worked perfectly.SO its not because of the multiplexing!! and its not the code. I think something is interfering or resetting the microcontroller because it does not store the values on the seven segments.The motors on the right are not connected. Any clue what is wrong?

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago in reply to rishi2628 +2
    RIshi, mcb1 told that there is a power problem NOT because the 7805 is a crap component but because, with a reasonable difficult we are trying to decode your info and seems that your schematic has issues…
  • mcb1
    mcb1 over 10 years ago in reply to balearicdynamics +2
    rishi2628 The syntax highlighting that Enrico is referring to is a little hidden. It's a shame there isn't a simple icon, but we struggled to get it added, so it's better than nothing. past you code, then…
  • clem57
    clem57 over 10 years ago +2
    Why do you automatically discount multiplexing? Just because it worked one place does not mean it works in ALL places... You could have affected other wires while hooking up from the old Uno. Many factors…
Parents
  • rishi2628
    0 rishi2628 over 10 years ago

    mcb1

    clem57

    balearicdynamics

    Robert Peter Oakes

     

    Ok here is the complete circuit with EVERYTHING. Please note a couple of things:-

    1) I have not used capacitors with 7805, hope it does not cause any problem.

    2)The 5 volt output from 7805 powers 2 pwm servos and the atmega328p microcontroller. It is also attached to the input buttons.

    3)Even when i detach the servos from the circuit , the flickering still happens which is evident from the video.

    4)I have attached 0.1uf capacitors to every switch including reset button to prevent debouncing.

    5)I am using analog pins as output pins

    6) Lastly if anybody hasn't seen the flickering problem them please visit the link below, and note that for 20 seconds it works ok, then the flickering start.

    https://www.youtube.com/watch?v=hdxqWKZSfso

     

    Now here is the complete circuit:-

    (please open it in new tab for a magnified image)

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to rishi2628

    Many thanks, Rishi!

     

    Well, first of all the power regulator without capacitors (and few other discrete components) is not the worth. At least it reduce the life of the battery, but it is very probable that one of the causes of the flickering depends on this, plus many other issues.

     

    About the problem os the regulator, it is very probable that you incur in the ripple  issue. Whenever current is drawn from a regulator the voltage will start to drop but it is needed an amount of time before the regulator start increasing the voltage to compensate.  This is the ripple effect.  The amount of ripple will be larger if more current is drawn from the regulator so I suppose that when the system starts things seems going well but then the performances decreases as time go ahead; tale in account that the LM7805 as all this kind of regulators compensate the current with temperature dispersion so as time passes the system tend to be hot and the effect is more visibile..  To compensate the ripple effect just a capacitor provides a temporary bank of energy.  This is used to keep the voltage stable.

     

    As source of inspiration please see the schematic in the image below.

     

    image

     

    Hope you are not offending if I prefer that this part is set correctly before we take in consideration more in depth the circuit. I think that your excessive simplification may really create serious unwanted behavior to your system.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to balearicdynamics

    brishisharma happy that you have solved the problem!!!

     

    Reading the past posts I see that wrote:

     

    Do you have a multimeter to check the voltages?

    If you are using a 7805, when they get hot they also start pulsing on and off so just check to make sure it's capable of supplying the current you need and also a temperature check while it's in operation would remove that doubt.

    but unfortunately we had not yet your full circuit image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to balearicdynamics

    brishisharma happy that you have solved the problem!!!

     

    Reading the past posts I see that wrote:

     

    Do you have a multimeter to check the voltages?

    If you are using a 7805, when they get hot they also start pulsing on and off so just check to make sure it's capable of supplying the current you need and also a temperature check while it's in operation would remove that doubt.

    but unfortunately we had not yet your full circuit image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 10 years ago in reply to balearicdynamics

    It's usually better to not power the servo's from the same source as the microcontroller but it is entirely possible with the right design. Most linear voltage regulator circuits should be built around a setup similar to the one balearicdynamics posted above with a small ceramic capacitor to smooth high frequency distortions and a larger electrolytic capacitor to provide extra power when needed.

     

    Moving on from, powering the servos from there directly and then placing a diode between there and your microcontroller with another capacitor after it will give your logic circuit it's own independent power reserve which would help prevent it from resetting during times of heavy load.

     

    I used this setup in one of my small robots that used 2 servo's powered from the same regulator as the logic and very rarely have power issues with it. They will occur if the servo's are pushed to their stall torque for any lengthy period of time but if thats happening then you should become more concerned over the possible damage to the serbo's and redesign the system around that.

     

     

    Lucie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to Former Member

    I agree with you. In the Tilt-pan camera I have provided a separate power line for the two servos that moves the camera stuff along the two axes. Then the micro controller when the program starts enable this line via a relais. This has also the advantage to use several types of servo leaving untouched both the software and circuit.