Arduino Forum What is the problem?
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
  • State Verified Answer
  • Replies 33 replies
  • Answers 3 answers
  • Subscribers 394 subscribers
  • Views 2141 views
  • Users 0 members are here
  • flickering
Related

What is the problem?

rishi2628
rishi2628 over 10 years ago

I have made the following circuit, can anyone please tell me why the seven segments are flickering. I have used multiplexing, don't tell me it is because of that. I have tried it prototyping on an arduino uno and it worked perfectly.SO its not because of the multiplexing!! and its not the code. I think something is interfering or resetting the microcontroller because it does not store the values on the seven segments.The motors on the right are not connected. Any clue what is wrong?

  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 10 years ago in reply to rishi2628 +2
    RIshi, mcb1 told that there is a power problem NOT because the 7805 is a crap component but because, with a reasonable difficult we are trying to decode your info and seems that your schematic has issues…
  • mcb1
    mcb1 over 10 years ago in reply to balearicdynamics +2
    rishi2628 The syntax highlighting that Enrico is referring to is a little hidden. It's a shame there isn't a simple icon, but we struggled to get it added, so it's better than nothing. past you code, then…
  • clem57
    clem57 over 10 years ago +2
    Why do you automatically discount multiplexing? Just because it worked one place does not mean it works in ALL places... You could have affected other wires while hooking up from the old Uno. Many factors…
Parents
  • rishi2628
    0 rishi2628 over 10 years ago

    image

     

    here is the working, and the blinking glitch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • billpenner
    0 billpenner over 9 years ago in reply to rishi2628

    The first step would have been to use a stable 12 volt supply instead of a battery. If the circuit worked it that point, the power supply does not have sufficient capability to drive the circuit. A voltmeter would also isolate the problem. A nine volt battery does not have very much capacity.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • billpenner
    0 billpenner over 9 years ago in reply to rishi2628

    The first step would have been to use a stable 12 volt supply instead of a battery. If the circuit worked it that point, the power supply does not have sufficient capability to drive the circuit. A voltmeter would also isolate the problem. A nine volt battery does not have very much capacity.