Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino USB powering Arduino and 3.3v device
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 421 subscribers
  • Views 2293 views
  • Users 0 members are here
  • arduino
Related

Arduino USB powering Arduino and 3.3v device

alexbee13
alexbee13 over 11 years ago

Hi. Im a newbie when it comes to this stuff but i recently bought an arduino and i was wondering if i could use the arduino cable and splice into it and connect the arduino using standard 5v then add a zener diode on another wire attatched to the 5v wire. Can i do this? I need a 3.3v power source and 5v for the arduino without using 2 usb cables. I know its probably the bad way of doing it. Im just curious to see if i can do it. Its the arduino uno.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 11 years ago in reply to alexbee13 +1
    No worries. I have annotated your drawing with my suggested approach. Forget about anything within the greyed out box area and consider adding the two wires I have added in:
  • screamingtiger
    screamingtiger over 11 years ago +1
    One thing being left out, the device you are powering. How much current will it draw? The 3.3 output o the arduino is rated for 50ma. If you need more I can see why you want to use the USB. I don't recommend…
Parents
  • gadget.iom
    0 gadget.iom over 11 years ago

    Which version of Arduino are you using?

    Many have a 3.3v pin on them that you could use.

     

    It's important to remember that the I/O on the Arduino will still be at 5v though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexbee13
    0 alexbee13 over 11 years ago in reply to gadget.iom

    Its the arduino Uno. i purchased from Maplins in UK yesterday. basically i was wondering if i can do this. i drew a diagram.image

    I appologise for the bad drawing but. can i do this. have the arduino and the Xbox 360 RF board (needs 3.3v) connected to 1 USB cable or will this cause problems?

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 11 years ago in reply to alexbee13

    No worries. I have annotated your drawing with my suggested approach.

    Forget about anything within the greyed out box area and consider adding the two wires I have added in:

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexbee13
    0 alexbee13 over 11 years ago in reply to gadget.iom

    that would be a better alternative. the only problem is that the RF module has 3.3v but you needed the zener diode to A) take it down to 3.3 and B) to prevent any voltage drops or something. it was to make sure the flow could only go to the Module and not come back. if i did that. i would risk burning the arduino out wouldnt i?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to alexbee13

    From USB is 5V nominal, with a 5.1V zener used as a zener it would drop the whole 5V and leave you nothing for the 3V3 board. A standard diode will drop about 0.7V so 5V would become about 4.3V but with USB it could be less or more than 5V.

     

    The diagram that paulellison shows is utilizing the 3.3V output already available from the UNO and that is regulated so is just right for the board it is connecting to

     

    The issue that is outstanding is if your device that is not specified can handle a logic 5V from the uno on its inputs and if not then there are a few simple possibilities you can use to integrate the UNO to your board. Without knowing the board it is hard to say. but options include

     

    A couple of resistors to divide the 5V into 3V3 so perhaps a 1Kand a 1.5K would work.

    2 diodes in series to drop about 1.4V has worked for many people

    a level shifter with a transistor and 2 resistors1K to the base of the transistor from the UNO output and 1K between the collector and the 3V3 rail. take the output from the collector to the board needing 3V3. the emitter is connected to 0V.

     

    all these of course assume your driving one way if the board needs 2 way then its a little different

     

    let us know what the other board is and we could better advise

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 11 years ago in reply to alexbee13

    From USB is 5V nominal, with a 5.1V zener used as a zener it would drop the whole 5V and leave you nothing for the 3V3 board. A standard diode will drop about 0.7V so 5V would become about 4.3V but with USB it could be less or more than 5V.

     

    The diagram that paulellison shows is utilizing the 3.3V output already available from the UNO and that is regulated so is just right for the board it is connecting to

     

    The issue that is outstanding is if your device that is not specified can handle a logic 5V from the uno on its inputs and if not then there are a few simple possibilities you can use to integrate the UNO to your board. Without knowing the board it is hard to say. but options include

     

    A couple of resistors to divide the 5V into 3V3 so perhaps a 1Kand a 1.5K would work.

    2 diodes in series to drop about 1.4V has worked for many people

    a level shifter with a transistor and 2 resistors1K to the base of the transistor from the UNO output and 1K between the collector and the 3V3 rail. take the output from the collector to the board needing 3V3. the emitter is connected to 0V.

     

    all these of course assume your driving one way if the board needs 2 way then its a little different

     

    let us know what the other board is and we could better advise

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 11 years ago in reply to Robert Peter Oakes

    I think he said:

     

    have the arduino and the Xbox 360 RF board (needs 3.3v) connected to 1 USB cable or will this cause problems?

    Does that change anything Robert Peter Oakes

    Clem