Arduino Forum Circuit Issue with MOSFET
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
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 394 subscribers
  • Views 2368 views
  • Users 0 members are here
  • irf540
  • 2N7000
  • arduino
Related

Circuit Issue with MOSFET

wallarug
wallarug over 10 years ago

Hey,

 

I am having issues with this circuit:

 

image

 

Background:  This circuit is to control an RGB LED strip (so three of the above would achieve this).  The reason for this particular design is: IRF540 to drive load (large current) and the two 2N7000 drive the MOSFET, reducing current drain from Controller (possibly a 3v3 Arduino).  The double 2N7000 allows the IRF540 to be active when logic high.

 

Can someone please tell me if there is a problem with the above schematic, otherwise I think it would be my breadboard layout is not correct. (too hard to post that right now).

 

Any comments would be much appreciated.

 

Many thanks,

 

wallarug

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 10 years ago +2
    How is it (mis)behaving? Just some ideas: 1. In general, don't hook up your actual output device until you're sure the circuits controlling it work with a voltmeter. Put a resistor in place of the LED…
  • wallarug
    wallarug over 10 years ago in reply to johnbeetem +1
    Thanks John, I will take everything above into consideration.
  • mcb1
    mcb1 over 10 years ago +1
    @wallarug I'm having feeling of dejavue with a similar circuit some time back to do a similar task. The first FET is right on the limit for conducting, so you could reduce the resistor to 1k or similar…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    You might want to have a little TV time image, yes im in them  but its better than coronation street (IMHO)

     

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/driving-big-loads-with-your-micro-controller--no-isolation

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/drive-big-things-with-added-safety-opto-isolators

    and for reading:-

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/sense-big-things-with-your-launchpad-or-arduino-opto-isolated-inputs

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    You might want to have a little TV time image, yes im in them  but its better than coronation street (IMHO)

     

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/driving-big-loads-with-your-micro-controller--no-isolation

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/drive-big-things-with-added-safety-opto-isolators

    and for reading:-

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/sense-big-things-with-your-launchpad-or-arduino-opto-isolated-inputs