Arduino Forum how could i create a network of arduinos?
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
  • State Not Answered
  • Replies 7 replies
  • Subscribers 392 subscribers
  • Views 907 views
  • Users 0 members are here
  • network
  • connection
  • microcontroller
  • arduino
Related

how could i create a network of arduinos?

Former Member
Former Member over 10 years ago

Hello All,

I am new to this page; i have been working on an arduino to capture information from a position sensor. Now i would like to use multiple sensors in different places, and for that i need to use multiple arduinos. i would like to connect them in the format of a network, not necessarily linear. i know if you want to connect a bunch of them in line you could create a bus line from V+ and GND, and for data from pins 4 and 5. but how would i make it a network? what would i need for that hardware and software related? how does the host/client work?

any help is much appreciated.

Karim

  • Sign in to reply
  • Cancel

Top Replies

  • gadget.iom
    gadget.iom over 10 years ago +2
    Have a look at this tutorial: How to Network Five Arduinos (or more) using I2C - TechBitar
  • gadget.iom
    gadget.iom over 10 years ago in reply to Former Member +1
    I would personally recommend a bus network over 485. This will give you a decent transmission distance. The master can then poll the sensors as necessary. This kind of infrastructure is popular, and popular…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to gadget.iom +1
    I agree with Paul on this, RS485 is a proven industry workhorse over considerable distances and for wireless there is both Sub Ghz radios that are very inexpensive and also simple WIFI in the form of the…
  • gadget.iom
    0 gadget.iom over 10 years ago

    Have a look at this tutorial:

    How to Network Five Arduinos (or more) using I2C - TechBitar

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to gadget.iom

    thank you; i had seen something very similar.

    my question is what if i wanted to branch out of one of the 4? what happens to the master/slave communication? essentially what i am wondering is that, is this network only supposed to work as a tree topology? could they not be mutually connected?

    i appreciate your help.

    Karim.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to Former Member

    I2C is typically connected in a bus configuration as shown in the linked tutorial.

    What do you mean by "mutually connected"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 10 years ago in reply to gadget.iom

    thank you; yes absolutely.

    what i meant was to have, as an example, a topology like this:

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 10 years ago in reply to Former Member

    I would personally recommend a bus network over 485. This will give you a decent transmission distance.

    The master can then poll the sensors as necessary. This kind of infrastructure is popular, and popular for a reason.

    Have you considered going wireless?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to gadget.iom

    I agree with Paul on this, RS485 is a proven industry workhorse over considerable distances and for wireless there is both Sub Ghz radios that are very inexpensive and also simple WIFI in the form of the ESP boards, also cheap and easy to use and very extendable over vast distances, did someone say across the otherside of the world image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to gadget.iom

    As a matter of fact IMHO the topology should be something like the USB hub architecture to you are covered for any needs and the bus really act as a bus. The selection bits are just to address multiple devices inside the same bus architecture.