Arduino Forum Help needed! Arduino output to app inventor 2 input via bluetooth.
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 389 subscribers
  • Views 269 views
  • Users 0 members are here
  • appinventor2
  • bluetooth
  • mit_app_inventor
  • arduino
  • input/output
Related

Help needed! Arduino output to app inventor 2 input via bluetooth.

Former Member
Former Member over 10 years ago

I need help figuring out how to revieve an input on an app inventor app from an arduino via bluetooth. i already have outputs from appinventor to arduino but now need to reverse that for about 5 inputs to the app. the problem is whatever i seem to do the app or arduino is not translating the data correctly and will not read the input and there for will not show a picture that it is suppose to when a certain input is recieved. Please help. Very important project for work and almost done! Nedd help ASAP!

 

here is the arduino code.

 

 

int AUTO = 13;

int pp = 12;

int slider = 11; //pwm

int manUp = 10;

int manDown = 9;

int cal = 8;

int value = 52;

int testButton1 = 2;

int val1 = 49;

String readString;

 

 

void setup()

{

  Serial.begin(9600);

  pinMode(AUTO, OUTPUT);

  pinMode(pp, OUTPUT);

  pinMode(slider, OUTPUT);

  pinMode(manUp, OUTPUT);

  pinMode(manDown, OUTPUT);

  pinMode(cal, OUTPUT);

  pinMode(testButton1, INPUT);

  analogWrite(slider, value); //default standoff = 1mm

  value = -1;

}

 

 

 

 

 

 

void loop()

{

  while (Serial.available())

  {

    delay(3);

    value = Serial.read();

    char c = Serial.read();

    readString += c;

    if (value >= 50)

    {

      Serial.println(value);

      analogWrite(slider, value);

 

 

    }

    if (value == 33)

    {

      digitalWrite(AUTO, HIGH);

    }

    if (value == 34)

    {

      digitalWrite(AUTO, LOW);

    }

    if (value == 36)

    {

      digitalWrite(pp, HIGH);

    }

    if (value == 37)

    {

      digitalWrite(pp, LOW);

    }

    if (value == 38)

    {

      digitalWrite(manUp, HIGH);

    }

    if (value == 39)

    {

      digitalWrite(manUp, LOW);

    }

    if (value == 40)

    {

      digitalWrite(manDown, HIGH);

    }

    if (value == 41)

    {

      digitalWrite(manDown, LOW);

    }

    if (value == 35)

    {

      digitalWrite(cal, HIGH);

      delay (200);

      digitalWrite(cal, LOW);

    }

  }

 

  val1 = digitalRead(testButton1);

  if (val1 == HIGH)

  {

    Serial.println(val1);

    delay(500);

  }

}

 

 

 

Heres the app.

 

 

image

  • Sign in to reply
  • Cancel
  • neilk
    0 neilk over 10 years ago

    Hi wsallee07

     

    Looking quickly at your AppInventor blocks of code, I can't decide if you are expecting to receive text or an unsigned 1 byte number - you appear to be trying to do both

     

    There are code blocks receiving for text and code blocks for receiving numbers in the Bluetooth section. I have never tried to mix them; I don't think it will work if you do.

     

    Hope this helps

     

    Neil