Arduino Forum 4 Channel 12V relay system issues.
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
  • State Verified Answer
  • Replies 33 replies
  • Answers 2 answers
  • Subscribers 394 subscribers
  • Views 8111 views
  • Users 0 members are here
Related

4 Channel 12V relay system issues.

screamingtiger
screamingtiger over 10 years ago

mcb1

I bought this relay system and it doesn't work 

http://www.ebay.com/itm/231573073495?_trksid=p2057872.m2749.l2649&ssPageName=STRK%3AMEBIDX%3AIT

 

Its a 12V relay system so I have to use 12V into the VCC and the input pins are driven by 5V.  So I connect 5V in, the relays trip.  The code is simple, digital high and low with a 1 second delay.  Pins are output.

The little LEDS turn off and on as expected but the relays do not trip.  I don't have a load on them but should not matter.  If I use 12V as required into the VCC, the leds only turn on, then go dimmer, never off.

I have a common ground between the arduino and relay board as well.

 

What is going on?

 

I went ahead and 2nd day aired a 5v version, I will just run it off the same regulator as the arduino.  Anybody have any experience with these?

 

<body><p>I bought this relay system and it doesn't work  <img ___jive_emoticon_name="sad" class="jive_macro jive_emote" jivemacro="emoticon" src="http://www.element14.com/community/images/emoticons/sad.gif"/></p><p><a href="http://www.ebay.com/itm/231573073495?_trksid=p2057872.m2749.l2649&ssPageName=STRK%3AMEBIDX%3AIT">http://www.ebay.com/itm/231573073495?_trksid=p2057872.m2749.l2649&ssPageName=STRK%3AMEBIDX%3AIT</a></p><p></p><p>Its a 12V relay system so I have to use 12V into the VCC and the input pins are driven by 5V.  So I connect 5V in, the relays trip.  The code is simple, digital high and low with a 1 second delay.  Pins are output.</p><p>The little LEDS turn off and on as expected but the relays do not trip.  I don't have a load on them but should not matter.  If I use 12V as required into the VCC, the leds only turn on, then go dimmer, never off.</p><p>I have a common ground between the arduino and relay board as well.</p><p></p><p>What is going on?</p><p></p><p>I went ahead and 2nd day aired a 5v version, I will just run it off the same regulator as the arduino.  Anybody have any experience with these?</p></body>
  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago +2 verified
    Joey Did you remove the jumper .. JD-VCC to VCC ? You apply the 12v to JD-VCC NOT THE VCC PIN The 5v on the VCC pin is to power the Optocouplers ... Also note that these turn on with a LOW so you need…
  • jw0752
    jw0752 over 10 years ago in reply to screamingtiger +2
    Hi Joey, From my experience you will probably find that the 12 V relays will close at about 8 volts and release around 3 or 4 volts. If you have a variable voltage supply you can test this for yourself…
  • mcb1
    mcb1 over 10 years ago in reply to screamingtiger +2
    but I do not have 3.3V any where Many of the optical mice have a 3v3 regulator inside (looks like a transistor) if you want to canabilise something. Some of the Arduino's have a 3v3 regulator onboard…
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    The jumper is to allow you to completly isolate the drive tothe relays  from the drive to the opto isolators if you want to

     

    The optos can probable work on any voltage from 5V to 12V, it is what you use to drive the optos that will limit this. If you use an ULN2003 for example then it will work with 5-12 easily, if your running directly from the output of a controller then it will be limited to 5V (Assuming a 5V controller output but it will have to be able to sink 10mA ish.

     

    With the jumper removed you will NOT connect the GND lead to the controller, you will feed the VCC with the supply that is common to the controller (5V for example) and the controller will sink the current to its ground when it wants the relay to turn on

     

    the relay power (12V) would be supplied to the JDVcc pin and the ground of the relay board will goto the ground of the 12V supply only

     

    this would keep the micro completly isolated from the relay power so less noise interfering with the micro controller.

     

    if you have the jumper in place then you can not fed the micro power (5V) to the board as it will not work at that voltage (Relays) and if you power the board with 12V you will need an intermediate driver that will level shift the 5V from the controller to 12V  (IE a ULN2003, Transistor or FET... your choice). see this video for additional info:

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/driving-big-loads-with-your-micro-controller--no-isolation

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/drive-big-things-with-added-safety-opto-isolators

    http://www.element14.com/community/groups/internet-of-things/blog/2014/08/05/sense-big-things-with-your-launchpad-or-arduino-opto-isolated-inputs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to Robert Peter Oakes
    These do not function at all at 5V nor 6.6V for if they did I would not of had any issue

    Might pay to read the whole post....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to mcb1

    image, did read...

    In my post im talking about driving the OPTO isolators from 5 - 12V, not the relays, I clearly say they need 12V and if you have the jumper in then you need 12V +  a level shifter image

     

    Back at ya image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • screamingtiger
    0 screamingtiger over 10 years ago in reply to Robert Peter Oakes

    He was talking to me.

     

    12V on the VCC did not work.  Which is odd considering is jumped to JD-VCC, even if I put 12V on the input pins.  I tried.

     

    In summary, with the jumper installed on the 12V relay system, the whole unit is useless, there is no configuration with the jumper installed that will work.  Even if you level shift the input, I tried.

     

    The input pins MUSt be 5V, no more.  VCC must be 5V, no more.  JD-Vcc must be 12V (or something close, I will test the lower limit but it is NOT 6.6V, that didn't fire them.)

     

    this is good information but keep in mine mine is a cheap Chinese knockoff, who knows how it was made and if it will behave as expected, we could discuss all day.  I could make a video proving each scenario, but that may only work for my specific unit!

     

    I still do not understand why the have a jumper when there are 12V relays and VCC cannot have more than 12V.  (If you put 12V the leds light up permanently while power is installed which is not a good sign)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago in reply to screamingtiger

    nope, your assesment is correct, relay voltage must be 12V nominal

     

    the rest is about sinking (NOT Sourcing) the opto input to gnd

     

    my previous post will work assuming nothing is broken

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to screamingtiger

    This is getting to be a long conversation ... but Joey is learning new things image

    and who knows who else is reading and also gaining knowledge.

     

     

     

    Robert Peter Oakes

    Joey put up a link and worded how he hooked it up.

    The one item that wasn't was the correct voltage to drive the relay which we have resolved.

     

    Why when you have an opto coupled input that will work from 5v (the series resistor is too high for 3v3) would you want to run it from 12v, THEN add a level converter to your 5v device.

    If there was no way of isolating the relay power from the driver, it would be useful, but in this case the images showed a jumper was available.

     

    Your suggestion is valid if someone posted a question about how best to use these cheap relay boards ...image

     

     

    screamingtiger

    Joey The control side can be anything from 5v to whatever.

    Most of these boards use a 1k ohm resistor in series with the opto and a LED, and hence at 5v the maximum current is approx 2.2mA (5v -1.4 - 1.4 (leds) = 2.2v  I=E/R = 2.2/1000 = 0.0022A or 2.2mA

    At 12v the current rises to 12-2.8 = 0.0092 or 9.2mA.

    The opto is capable of 50mA but I doubt the series LED is..image

     

    You do need to be aware of the device that is controlling the opto side. You have to ensure it doesn't have a voltage that exceeds its limits applied to it.!

    (GOLDEN RULE ... never apply a voltage to a pin that is greater than the supply UNLESS it is designed for it.)

     

    If you do stick 12v on a 5v device, depending on the device and its internal design, it might conduct this to the Vcc to protect itself.

     

    In the case of your opto board, if you draw current through the control pin, current flows from the Relay Board Vcc rail, through the series resistor, optocoupler (and indicator LED).

    This will cause the LED inside the opto to illuminate and turn on the output side.

     

    why the have a jumper when there are 12V relays and VCC cannot have more than 12V.

    With the above in mind this statement is wrong.

     

    If you want to prove this for yourself at some time.

    • Discconect it from your Arduino .!
    • Apply 12v to the VCC with the JD-VCC to VCC jumper in place and the ground of your 12v source connected to the ground connection.
    • Short any of IN1-IN4 to ground, and the correspnding led will light and the relay should be operated.

     

    If that doesn't work you better include a good photo of the top and bottom of the board as it would appear your little asian friends have got the wrong schematic ...

     

    WHY make them like this

    Many devices have Open Collector outputs, or use a transistor to do the switching. (those cheap PIR's do exactly this with a small resistor in series)

    The collector of the transistor connects to IN1-IN4 and when its ON the opto is ON which turns on the relay.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • screamingtiger
    0 screamingtiger over 10 years ago in reply to mcb1

    I see what I said wrong, I mean that there is not configuration that will work with the jumper, using a 5V micro controller!  These are designed for micro controllers and I am not aware of one that will work with 12V.  I guess there would be a way with mosfet to sink it to ground or I could use a relay to sink the pin to ground, and that's the point.  To use 12V you would have to use another "relay" (fet etc..) to make the relay board work, makes 0 sense.  I need a relay board to operate the relay board.

     

    I actually did it wrong anyways and attempted to source 12v on the IN pins instead of sink it to ground.  I didn't try that. 

     

    And no I didn't read the shematic.  Could I?  Yes, I used to solve circuits all the time with passive and active components in college.  But that is 12 years ago... image   I need to get back into it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to screamingtiger

    But that is 12 years ago...

    It's like riding a bike ... wobbly at first, then fine (well until certain parts get sore).

     

    As jw0752 pointed out the schematic is seriously flawed ...with the shorted coil and the reverse LED nothing would work...image

     

    I guess there would be a way with mosfet to sink it to ground

    a small signal transistor will work fine ....

     

    You need to keep in mind that these aren't built just for 5v micros ...

    Some of them have 5v relays.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to mcb1

    Just a stupid question inside all this discussion. Why do you have not built your own? It seems almost a simple circuit.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to balearicdynamics

    Why do you have not built your own?

    Sorry what bit are your referring to.?

     

    In NZ we usually wire our trailers with a plug.

    The common version (last 15 years) is a 7 pin that has captive lugs that the socket door holds onto.

    NARVA Trailer Plug 7 Pin Flat Quickfit Plastic  NARVA Trailer Socket 7 Pin Flat Quickfit Plastic   image

    so the wireless isn't needed.

     

    For the relay boards, I've used them as they are but most of mine were 5v coils.

     

    Is that what you were meaning ??

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to mcb1

    Sounds a great solution Mark. Should investigate for my applications image

     

    I mean that if this board has lot of problems and so few documentation and so on, why not to build a simple board. It has only i opto + three SMD components (maybe replaced by through the hole, seems discrete ones only) and a relay. It seems to me that all the advantages of the probably very cheap all-built has been lost in time to understand the issues and how the circuit works.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to mcb1

    Sounds a great solution Mark. Should investigate for my applications image

     

    I mean that if this board has lot of problems and so few documentation and so on, why not to build a simple board. It has only i opto + three SMD components (maybe replaced by through the hole, seems discrete ones only) and a relay. It seems to me that all the advantages of the probably very cheap all-built has been lost in time to understand the issues and how the circuit works.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 10 years ago in reply to balearicdynamics

    if this board has lot of problems and so few documentation and so on, why not to build a simple board

    I think that it's more the vendor had poor support information.

     

    Terry King sells almost the same device, but he provides all the supporting documentation, etc.

    http://yourduino.com/sunshop2/index.php?l=product_detail&p=201

    why not to build a simple board

    At that sort of price ..why would you even bother

     

    Sadly Joey was still learning, and hence had the issues ...and that's totally understandable

    I've used a very similar one on a Raspberry Pi and simply added a 1k ohm across the 1K so it works on 3v3.

    image

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to mcb1

    We all are still learning. Or died image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • screamingtiger
    0 screamingtiger over 10 years ago in reply to mcb1

    mcb1 wrote:

     

     

     

    Sadly Joey was still learning, and hence had the issues ...and that's totally understandable

    I've used a very similar one on a Raspberry Pi and simply added a 1k ohm across the 1K so it works on 3v3.

     

     

     

     

    Sadly?  Is it that bad LOL?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 10 years ago in reply to screamingtiger

    Oh, Joey, it's so bad.

     

    I was sure you was a natural born engineern LOL image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to screamingtiger

    Sadly?  Is it that bad LOL?

    No not all all ... it was the wrong word choice ...sorry.