Arduino Forum Arduino - Sink more than 6 volts
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
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 405 subscribers
  • Views 433 views
  • Users 0 members are here
  • arduino
Related

Arduino - Sink more than 6 volts

Former Member
Former Member over 10 years ago

Hi everyone,

 

I need to sink an active low line in a system to ground using an Arduino, the problem is that it's more than what the Arduino's pins can handle around 6v. I tried finding out if a mosfet would actually connect Drain to Source and drive the line low (ground) and just drive the gate with the arduino, but I couldn't find anything, or at least didn't understand it.

 

Thanks for any help! image

 

Regards

 

Theoneil

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago +1 suggested
    The goto IC for that kind of thing the low cost, available everywhere ULN2003 http://www.ti.com/lit/ds/symlink/uln2003a.pdf up to 50V and upto 1000mA peak, 500mA typical, you can combine pins if you need…
Parents
  • gdstew
    0 gdstew over 10 years ago

    The 7406 is a hex (6) inverting buffers and the 7407 is the non-inverting version of these TTL ICs that are still easy to find and will handle

    up to 30V @ 20 mA (you didn't mention how much current you needed to handle). They are available in 14 pin DIP packages and are easy

    to use. You should ground all non-used inputs,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gdstew
    0 gdstew over 10 years ago

    The 7406 is a hex (6) inverting buffers and the 7407 is the non-inverting version of these TTL ICs that are still easy to find and will handle

    up to 30V @ 20 mA (you didn't mention how much current you needed to handle). They are available in 14 pin DIP packages and are easy

    to use. You should ground all non-used inputs,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer