Arduino Forum Euro sign
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
  • Replies 13 replies
  • Subscribers 392 subscribers
  • Views 2012 views
  • Users 0 members are here
Related

Euro sign

ritamüller
ritamüller over 10 years ago

Hallo,

 

How can I enter Euro sign with Serial.print?

 

 

Thx

Rita

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller +1
    Your routine that is called print() always puts a new line before it exits therefor your euro symbol will always be on a new line. remove this from the print routine and put the newline statements elsewhere…
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller +1
    My assumption about the board is correct, it shares the serial (USB) between the PC console and the RFID reader and therefor you will not be able to eliminate the garbage looking text if you look closly…
Parents
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    or to make it really simple

    void setup() {
      Serial.begin(9600);
      }
      Serial.println("Printing the Euro symbol");
    }
    int thisByte = 128;
    
    void loop() {
      Serial.write(thisByte);
    delay(1000);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago

    or to make it really simple

    void setup() {
      Serial.begin(9600);
      }
      Serial.println("Printing the Euro symbol");
    }
    int thisByte = 128;
    
    void loop() {
      Serial.write(thisByte);
    delay(1000);
    }

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ritamüller
    ritamüller over 10 years ago in reply to Robert Peter Oakes

    Hallo Peter ,

    Thanks for reply.


    Rita            

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ritamüller
    ritamüller over 10 years ago in reply to Robert Peter Oakes

    Hallo Peter ,

     

    do you know how I get the Euro sign in same row with the Price ?

    why I get gobbledygook letter in my Serial monitor ?

     

    image

     

    Thx

     

    Rita

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller

    Can you provide the sketch you are running for this

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ritamüller
    ritamüller over 10 years ago in reply to Robert Peter Oakes

    Hallo Peter ,

    here is my sketch :

     

    /*
    * RFID/NFC module for Arduino. 
    * Calculation the total price  
    */
    
    
    uint8_t dataRX[35];//Receive buffer.
    uint8_t dataTX[35];//Transmit buffer. 
    uint8_t _UID[4];// stores the UID (unique identifier) of a card.
    uint8_t keyAccess[] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF } ;// stores the key or password.
    uint8_t address = 0x04;//Address to read.
    uint8_t ATQ[2];//Answer to request
    uint8_t state;//state of the process
    uint8_t aux[16];//Auxiliar buffer. 
    unsigned int TotalPrice = 0;// Varialbe
    
    
    
    
    void setup()
    {
       //Start serial port 115200 bps:
       Serial.begin(115200);
       delay(100);
       Serial.print("Welcome dear customer");
       delay(1000);
       //!It is needed to launch a simple command to sycnchronize
       getFirmware();
       configureSAM();
    }
    int thisByte = 128;
    
    
    void loop()
    {
       Serial.print("\n");
       /////////////////////////////////////////////////////////////
       //Get the UID Identifier
       init(_UID, ATQ);
       Serial.print("\n");
       /////////////////////////////////////////////////////////////
       //Auntenticate a block with his keyAccess
       state = authenticate(_UID, address, keyAccess);
       Serial.print("\n");
    
    
       if ( state == 0) {
          Serial.println("Authentication block OK");
       } else {
       Serial.println("Authentication failed");
       }
       /////////////////////////////////////////////////////////////
       //Read from address after authentication
       state = readData(address, aux);
       Serial.print("\n");
    
    
       if (state == 0) {
          Serial.println("Read Price ok ");
       } else {
          Serial.println("Read failed");
       }
    
    
       Serial.print("\n");
       Serial.print("Price : ");
       print(aux ,1); 
       Serial.write(thisByte);
       Serial.print("\n");
       delay(2000);
    
    
    // Tota l price 
    
    
      TotalPrice = TotalPrice + aux[0]; 
      Serial.print("TotalPrice : "); 
      Serial.println(TotalPrice,1);
      Serial.write(thisByte);
      delay(1000);
    }
    
    
    //**********************************************************************
    //!The goal of this command is to detect as many targets (maximum MaxTg)
    // as possible in passive mode.
    uint8_t init(uint8_t *UID , uint8_t *ATQ)   //! Request InListPassive
    {
      Serial.flush();
    
    
       dataTX[0] = 0x04; // Length
       lengthCheckSum(dataTX); // Length Checksum
       dataTX[2] = 0xD4;
       dataTX[3] = 0x4A; // Code
       dataTX[4] = 0x01; //MaxTarget
       dataTX[5] = 0x00; //BaudRate = 106Kbps
       dataTX[6] = 0x00; // Clear checkSum position
       checkSum(dataTX); 
    
    
       sendTX(dataTX , 7 ,23);
    
    
       for (int i = 17; i < (21) ; i++){
          _UID[i-17] = dataRX[i];
       UID[i-17] = _UID[i-17];
       }
    
    
       ATQ[0] = dataRX[13];
       ATQ[1] = dataRX[14];
    
    
       if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x4B) & (dataRX[11] == 0x01)) {
          return 0;
       } else {
          return 1;
       }
    }
    //**********************************************************************
    //!A block must be authenticated before read and write operations
    uint8_t authenticate(uint8_t *UID, uint8_t blockAddress, uint8_t *keyAccess)
    {
       dataTX[0] = 0x0F;
       lengthCheckSum(dataTX);
       dataTX[2] = 0xD4;
       dataTX[3] = 0x40; // inDataEchange
       dataTX[4] = 0x01; //Number of targets
       dataTX[5] = 0x60; // Authentication code
       dataTX[6] = blockAddress;
       for (int i = 0; i < 6 ; i++) {
          dataTX[i + 7] = keyAccess[i];
       }
       dataTX[13] = UID[0];  dataTX[14] = UID[1];
       dataTX[15] = UID[2];  dataTX[16] = UID[3];
       dataTX[17] = 0x00;
       checkSum(dataTX);
       sendTX(dataTX , 18 ,14);
    
    
       if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
          return 0;
       } else {
          return 1;
       }
    }
    //**********************************************************************
    //!Write 16 bytes in address .
    uint8_t writeData(uint8_t address, uint8_t *blockData)  //!Writing
    {
       Serial.print("                ");
       dataTX[0] = 0x15;
       lengthCheckSum(dataTX); // Length Checksum
       dataTX[2] = 0xD4;
       dataTX[3] = 0x40;//inDataEchange CODE
       dataTX[4] = 0x01;//Number of targets
       dataTX[5] = 0xA0;//Write Command
       dataTX[6] = address; //Address      
    
    
       for (int i = 0; i < 16; i++) {
          dataTX[i+7] = blockData[i];
       }
    
    
       dataTX[23] = 0x00;
       checkSum(dataTX);
       sendTX(dataTX , 24 ,14);      
    
    
       if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
          return 0;
       } else {
          return 1;
       }
    }
    //**********************************************************************
    //!Read 16 bytes from  address .
    uint8_t readData(uint8_t address, uint8_t *readData) //!Reading
    {
       Serial.print("                ");
    
    
       dataTX[0] = 0x05;
       lengthCheckSum(dataTX); // Length Checksum
       dataTX[2] = 0xD4; // Code
       dataTX[3] = 0x40; // Code
       dataTX[4] = 0x01; // Number of targets
       dataTX[5] = 0x30; //ReadCode
       dataTX[6] = address;  //Read address
       dataTX[7] = 0x00;
       checkSum(dataTX);
       sendTX(dataTX , 8, 30);
       memset(readData, 0x00, 16);  
    
    
       if ((dataRX[9]== 0xD5) & (dataRX[10] == 0x41) & (dataRX[11] == 0x00)) {
          for (int i = 12; i < 28; i++) {
             readData[i-12] = dataRX[i];
          }
          return 0;
       } else {
          return 1;
       }
    }
    //**********************************************************************
    //!The PN532 sends back the version of the embedded firmware.
    bool getFirmware(void)  //! It is needed to launch a simple command to sycnchronize
    {
      Serial.print("                ");
    
    
       memset(dataTX, 0x00, 35);
       dataTX[0] = 0x02; // Length
       lengthCheckSum(dataTX); // Length Checksum
       dataTX[2] = 0xD4; // CODE
       dataTX[3] = 0x02; //TFI
       checkSum(dataTX); //0x2A; //Checksum   
    
    
       sendTX(dataTX , 5 , 17);
       Serial.print("\n");
       Serial.print("Your Firmware version is : ");
    
    
       for (int i = 11; i < (15) ; i++){
          Serial.print(dataRX[i], HEX);
          Serial.print(" ");
       }
       Serial.print("\n");
    }
    
    
    //**********************************************************************
    //!Print data stored in vectors .
    void print(uint8_t * _data, uint8_t length)
    {
       for (int i = 0; i < length ; i++){
          Serial.print(_data[i], HEX);
          Serial.print(" ");
       }
       Serial.print("\n");
    }
    //**********************************************************************
    //!This command is used to set internal parameters of the PN532,
    bool configureSAM(void)//! Configure the SAM
    {
       Serial.print("               ");
    
    
       dataTX[0] = 0x05; //Length
       lengthCheckSum(dataTX); // Length Checksum
       dataTX[2] = 0xD4;
       dataTX[3] = 0x14;
       dataTX[4] = 0x01; // Normal mode
       dataTX[5] = 0x14; // TimeOUT
       dataTX[6] = 0x00; // IRQ
       dataTX[7] = 0x00; // Clean checkSum position
       checkSum(dataTX);
    
    
       sendTX(dataTX , 8, 13);
    }
    //**********************************************************************
    //!Send data stored in dataTX
    void sendTX(uint8_t *dataTX, uint8_t length, uint8_t outLength)
    {
       Serial.print(char(0x00));
       Serial.print(char(0x00));
       Serial.print(char(0xFF)); 
    
    
       for (int i = 0; i < length; i++) {
          Serial.print(char(dataTX[i]));
       }
    
    
       Serial.print(char(0x00));
       getACK();
       waitResponse();// Receive response
       getData(outLength);
    }
    //**********************************************************************
    //!Wait for ACK response and stores it in the dataRX buffer
    void getACK(void)
    {
       delay(5);
       waitResponse();
       for (int i = 0; i < 5 ; i++) {
          dataRX[i] = Serial.read();
       }
    }
    //**********************************************************************
    //!Wait the response of the module
    void waitResponse(void)
    {
       int val = 0xFF;
       int cont = 0x00;
       while(val != 0x00) { //Wait for 0x00 response
          val = Serial.read();
          delay(5);
          cont ++;
       }
    }
    //**********************************************************************
    //!Get data from the module
    void getData(uint8_t outLength)
    {
       for (int i=5; i < outLength; i++) {
          dataRX[i] = Serial.read();//read data from the module.
       }
    }
    //**********************************************************************
    //!Calculates the checksum and stores it in dataTX buffer
    void checkSum(uint8_t *dataTX)
    {
       for (int i = 0; i < dataTX[0] ; i++) {
          dataTX[dataTX[0] + 2] += dataTX[i + 2];
       }
       byte(dataTX[dataTX[0] + 2]= - dataTX[dataTX[0] + 2]);
    }
    //**********************************************************************
    //!Calculates the length checksum and sotres it in the buffer.
    uint8_t lengthCheckSum(uint8_t *dataTX)
    {
       dataTX[1] = byte(0x100 - dataTX[0]);
    }

     

    Regards

     

    Rita

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller

    Your routine that is called print() always puts a new line before it exits therefor your euro symbol will always be on a new line. remove this from the print routine and put the newline statements elsewhere if you need them

    1. //********************************************************************** 
    2. //!Print data stored in vectors . 
    3. void print(uint8_t * _data, uint8_t length) 
    4. { 
    5.    for (int i = 0; i < length ; i++){ 
    6.       Serial.print(_data[i], HEX); 
    7.       Serial.print(" "); 
    8.    } 
    9.    Serial.print("\n"); 
    10. } 
    11. //********************************************************************** 

     

    also where you do this

    1.   Serial.println(TotalPrice,1); 
    2.   Serial.write(thisByte); 

    Serial.println vs Serial.print, the first one adds a new line before executing the next line so again adding a new line before you get to send the euro symbol, the second version does not so change your statement to the second version


    The other stuff is because your talking to your PN532 on the same serial as the console, or atleast that is what it seems so when you do things like sendTX(...) it will show up on the console, as this is not really printable ascii it looks like gobbledygook


    Provide your wireing schematic and or a link to the exact product your connecting and I can probably help further, I am assuming your using one of the ADAFRUIT boards but you dont say and are not showing any libraries so im guessing


    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ritamüller
    ritamüller over 10 years ago in reply to Robert Peter Oakes

    Hi Peter ,

    Thanks for the tip I have now the Euro sign with prices in the same row.

    I have RFID 13.56 MHz / NFC Module for Arduino from Cooking Hacks https://www.cooking-hacks.com/documentation/tutorials/rfid-13-56-mhz-nfc-module-arduino-raspberry-pi-tutorial/#step3


    Regards


    Rita

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller

    Can you mark the appropriate answers as correct / helpful, it helps me and others who help in the community attain the badges, thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller

    My assumption about the board is correct, it shares the serial (USB) between the PC console and the RFID reader and therefor you will not be able to eliminate the garbage looking text

     

    if you look closly on their site via your provided link, they have deliberatly dimmed out all the garbage to highlite the other text but it is still there and so even they acknowledge it is an issue (Expected behaviour)

     

    the only easy way around this would be to use an LCD display or something on the I2C but or using other GPIO pins to seperate the Human communications from the RFID communications. based on what I am seeing you do here, i dont think that would be too much of a challange for you

     

    regards

     

    Peter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ritamüller
    ritamüller over 10 years ago in reply to Robert Peter Oakes

    Hello Peter ,

    how can I make the answers as correct sign ?

     

    Rita

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to ritamüller

    usually it is pretty clear on the page but I just noticed this was posted as a discussion, not a question so perhaps that is why it is not showing