Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Best practices for Arduino I/O selection
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 414 subscribers
  • Views 5294 views
  • Users 0 members are here
  • arduino_development_environment
  • arduino
Related

Best practices for Arduino I/O selection

colporteur
colporteur over 4 years ago

I'm currently working on a project using an Arduino knock-off Mega board. I discovered during prototype board development and testing an issue using I/O' 0 and 1. I found I could not control the output within my script. From online research, I discovered if I was using serial communication then I should avoid using those two I/O's. I wonder what other gotcha's don't know about?

I confess I am way down the scale of Arduinos knowledge. I label myself more of a resurrectionist rather than a programmer. I adapt code and solutions I find to solve my problems. Rarely if ever, have I built from scratch. This leads me to the title line "Best Practices for Arduino I/O selection". Are there any resources that provide this type of guidance? Are there I/O's to avoid and others that are better for a specific function?

I realize some I/O's are for specific purposes. I'm just thinking are there best practices using I/O's. I read the review posted on the site of this new book and thought maybe that has some suggestions. I'm looking for member experience.

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 4 years ago in reply to shabaz +7
    I use the same principles but the other way round. I first do the inflexible ones, like UART, i2c/SPI, pwm/timer , interrupt and analogue. Then sprinkle the easy ones across what's left over.
  • fmilburn
    fmilburn over 4 years ago +7
    I've been caught out with this type of problem when using the Arduino IDE with a board I'm unfamiliar with so I can relate. In your case, the pins with the labels 0 and 1 on the silkscreen will cause a…
  • shabaz
    shabaz over 4 years ago +5
    Hi Sean, The usual board pinout diagrams often indicate all functions available per pin, so they can be used for guidance, but the ultimate authority is the chip datasheet. Example snippet (found via…
Parents
  • beacon_dave
    beacon_dave over 4 years ago

    On the Arduino Mega the first UART is wired to the 16U2 which connects you via USB to the host computer.

     image

    https://docs.arduino.cc/static/90b1ec517675fa8610166a1199868f51/A000067-datasheet.pdf

    The full pinout gives an overview of what the various pins are shared with
    https://docs.arduino.cc/static/edb006e0a180e80b9ea9cf8b4859dcd4/A000067-full-pinout.pdf

    Not all pins have PWM so perhaps one to watch out for and only a subset of the digital I/O are connected to the analogue multiplexer.

    Arduino uses some of the on-chip timers so need to be careful there
    Timer 0 - delay(), millis(), micros()
    Timer 1 - servo library
    Timer 2 - tone library
    /products/arduino/f/forum/39162/how-do-you-know-what-resources-timers-and-such-are-being-used-in-a-sketch

    Arduino hardware resource map
    https://code.google.com/archive/p/arduino/wikis/HardwareResourceMap.wiki

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to beacon_dave

    Good reminder.. software libraries can matter as you say, and sometimes they are coded or tested more on some pins too! even if theoretically they should work : ) All a balancing act factoring all that in, as well as any future project modification aspirations, e.g. swapping out a display to a different one, is easier if both displays/libraries of code are considered and so on.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 4 years ago in reply to beacon_dave

    Good reminder.. software libraries can matter as you say, and sometimes they are coded or tested more on some pins too! even if theoretically they should work : ) All a balancing act factoring all that in, as well as any future project modification aspirations, e.g. swapping out a display to a different one, is easier if both displays/libraries of code are considered and so on.