Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Single phase and three phase Induction Motor control arduino
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 414 subscribers
  • Views 3027 views
  • Users 0 members are here
Related

Single phase and three phase Induction Motor control arduino

e14 Contributor
e14 Contributor over 4 years ago

How do I control AC single phase 1/2hp @230v induction motor with arduino? Microcontroller should turn ON motor when water in a tank reaches below certain level and it should turn OFF motor when water in tank reaches above certain level.

  1. How to interface AC single phase as well as three phase induction motor with arduino or any other Microcontroller? 
  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 4 years ago +3
    I have had success controlling higher AC voltage devices with this solid state relay. https://www.banggood.com/80A-SSR-80DA-Solid-State-Relay-Module-DC-To-AC-24V-380V-Output-p-1097188.html?cur_warehouse…
  • robogary
    robogary over 4 years ago +2 suggested
    Use a small pilot relay driven by the Arduino to drive the coil of a bigger relay or contactor that feeds the power to the pump. Either relay is likely to be an industrial rated component. Some type…
  • dougw
    dougw over 4 years ago +1
    A simple and safe way is to buy a wireless remote switch and connect your microcontroller to the wireless remote controller. However a simple float switch at the each level could do the same job with…
Parents
  • phoenixcomm
    0 phoenixcomm over 4 years ago

    while Dougs's is overkill, and really nobody got it right, the problem with a float switch as when they are down they are "OFF" which is backwards for you. I worked for a while in a marble fabrication, and my header tank always ran ou of water and I would have to re-prime the damn thing. the easiest thing is ultrasonic module to a cheap Arduino and the output goes to a solid state relay. 

    Crs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • phoenixcomm
    0 phoenixcomm over 4 years ago

    while Dougs's is overkill, and really nobody got it right, the problem with a float switch as when they are down they are "OFF" which is backwards for you. I worked for a while in a marble fabrication, and my header tank always ran ou of water and I would have to re-prime the damn thing. the easiest thing is ultrasonic module to a cheap Arduino and the output goes to a solid state relay. 

    Crs