Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum L293d motor driver
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 414 subscribers
  • Views 3377 views
  • Users 0 members are here
Related

L293d motor driver

Kaushik_ma
Kaushik_ma over 4 years ago

So guys I had setup of rc car .I am using 4 motors , l293d driver ,ardunio Uno board and an hc -06 Bluetooth module for connection. The problem is after setting all if I supply current through batteries the l293d driver and ardunio is working but Bluetooth module is not working , instead I am giving the supply from power Bank the Bluetooth module and ardunio are running but l293d driver is not working..please tell me an solution

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +2 verified
    Can you show a photo or drawing of how power is connected?
  • ralphjy
    ralphjy over 4 years ago +2
    Have you tried removing the shield power jumper and powering the Arduino and the motors separately? You mentioned using a Power Bank. If this is a USB Power Bank, it will not power the motors (except…
  • shabaz
    shabaz over 4 years ago +2
    You're brave, constructing a battery pack from three LiPo cells that are unprotected according to the peeled one, into a cheap spring holder with thin wires. If there's a stall on the motors then expect…
Parents
  • dougw
    +1 dougw over 4 years ago

    Can you show a photo or drawing of how power is connected?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Kaushik_ma
    0 Kaushik_ma over 4 years ago in reply to dougw

    If I given power supply through 3 18650 batteries then expect Bluetooth module all are working and instead if I supplied power through power Bank then all are working except l293d motor driver

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 4 years ago in reply to Kaushik_ma

    18650 batteries are at least 3.7 V each - in series they would supply over 11V.  The regulator on an Uno can take this voltage, but a HC06 expects to run off 3-5V depending on the model. 5V is available on Uno pins, but 5V and GND need to be connected to the HC06 assuming it is the type with its own regulator. The motor driver may handle the higher voltage - you should check. A power bank may only supply 5 V which is fine for the UNO and HC06 but may not be enough for the motors. If you connect a power bank to the UNO USB port - it may not supply power to the motor controller. You need to supply the correct voltage to the UNO, the HC06 and the motor controller, and all grounds need to be connected together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 4 years ago in reply to Kaushik_ma

    18650 batteries are at least 3.7 V each - in series they would supply over 11V.  The regulator on an Uno can take this voltage, but a HC06 expects to run off 3-5V depending on the model. 5V is available on Uno pins, but 5V and GND need to be connected to the HC06 assuming it is the type with its own regulator. The motor driver may handle the higher voltage - you should check. A power bank may only supply 5 V which is fine for the UNO and HC06 but may not be enough for the motors. If you connect a power bank to the UNO USB port - it may not supply power to the motor controller. You need to supply the correct voltage to the UNO, the HC06 and the motor controller, and all grounds need to be connected together.