Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Does Arduino have a Dead Man switch?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 23 replies
  • Subscribers 410 subscribers
  • Views 5731 views
  • Users 0 members are here
  • arduino coding
  • arduino
Related

Does Arduino have a Dead Man switch?

colporteur
colporteur over 4 years ago

A dead man's switch is a device used as a fail-safe. These switches are usually used as a form of fail-safe where they stop a machine with no operator from a potentially dangerous action or incapacitate a device as a result of accident, malfunction, or misuse. 

I'm looking for some method to stop an Arduino to prevent harm. Is there an Arduino code sequence that will stop an Arduino and the only way to recover is to restart the device?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 4 years ago +10
    Watchdog circuits are the most common way to respond to serious system failure or software issues but there are a bunch of similar but subtly different concepts to clarify before a full answer... Fail…
  • robogary
    robogary over 4 years ago +5
    An ESTOP switch is a fail safe electro-mechanical device to provide fail-safe whether a machine is operating or not. A deadman switch is used when a machine is in operation to ensure the operator is…
  • javagoza
    javagoza over 4 years ago +5
    I recently faced a similar issue with the Arduino Nano 33 IoT. The Arduino Nano 33 IoT uses the 32-bit SAMD21 Arm Cortex-M0 processor so the solution would not work for all Arduino models. I had to activate…
Parents
  • robogary
    0 robogary over 4 years ago

    An ESTOP switch is a fail safe electro-mechanical device to provide fail-safe whether a machine is operating or not.

    A deadman switch is used when a machine is in operation to ensure the operator is in control.  

    In either case, a fail-safe solution is usually both hardware and software, often multiple layers of redundancy are used to reduce the chance that a fail-safe would fail to protect.  For example, an ESTOP/deadman  would implement an immediate stop in software (regen the motor in current limit), and remove power on a brake coil to cause the brake to set on a motor shaft. 

    If safety is a true concern, kill the Arduino power, and have an external means to release stored energy in the mechanical device and ensure safety, based on the risk.  

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • robogary
    0 robogary over 4 years ago

    An ESTOP switch is a fail safe electro-mechanical device to provide fail-safe whether a machine is operating or not.

    A deadman switch is used when a machine is in operation to ensure the operator is in control.  

    In either case, a fail-safe solution is usually both hardware and software, often multiple layers of redundancy are used to reduce the chance that a fail-safe would fail to protect.  For example, an ESTOP/deadman  would implement an immediate stop in software (regen the motor in current limit), and remove power on a brake coil to cause the brake to set on a motor shaft. 

    If safety is a true concern, kill the Arduino power, and have an external means to release stored energy in the mechanical device and ensure safety, based on the risk.  

    • Cancel
    • Vote Up +5 Vote Down