Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When is the function delay() a delay?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 413 subscribers
  • Views 10563 views
  • Users 0 members are here
  • delay
  • arduino_code
Related

When is the function delay() a delay?

colporteur
colporteur over 3 years ago

else if (MainDepartureState == LOW && MainArrivalState == LOW) {
        if (startupMain == HIGH) {
          // pulse turnout for Main train
          digitalWrite(Main_Turnout, HIGH);
          relayDelay();//<-----1
          digitalWrite(Main_Turnout, LOW);
          if (deBug == HIGH) {
            Serial.println("The Main Turnout Activated");
          }
          // Engage Motor for Main
          motors.setSpeedB(minSpeedB);  // Start Motor for Main
          motors.forwardB();
          PowerMain = LOW;
          startupMain = LOW;
          delay(300000);//<----2
          if (deBug == HIGH) {
            Serial.println("Motor Delay Complete");
          }

According to what I have read “The delay() function allows you to pause the execution of your Arduino code for a specified period.”

Why are the delays I am using not working or the values are so extreme? How can I best accomplish a delay?

I tried using the delay() function at point <----1 in my code and it failed miserably. I wanted to activate a relay by turning it on, waiting for relay to engage (delay(2000), then turn it off. The delay(2000) two seconds didn’t work. I wrote a little relay routine that accomplish what I wanted but why did delay(2000) not give me two seconds?

I am using delay() function at <----2 in the code but the value doesn’t reflect the actual delay. I needed to generate some wait time for the motor to engage and trigger a sensor. My desire was a three second delay(3000) but the delay(300000) was a value that actually worked. That would be 300 seconds yes/no?

I'm a code resurrectionist and not an actual programmer. I will try and muddle through discussions 

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +6
    Based on GL shared insight, I used a different set of PWM pins so as not to muck with the delay() timer. I also took the BE suggestions and used subtraction in the millis routines. I am happy to report…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +5
    //user input variables int turnout_delay = 10000; //delay for relay contacts to engage int motor_delay = 900000; //delay for motor to move train unsigned long time_now = 0; int type cannot store outside…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +3
    I think that it helps if one can see names like "TCCR0B" and know inside that it is short for "Timer Control Counter Register" then that should immediately set-off alarm bells in one's head. Gough Lui…
Parents
  • colporteur
    colporteur over 3 years ago

    I am going to put aside my reservation about posting full code and look to the baldengineer's suggestion  I somewhat suspect the old adage: "code snippets rarely contain the problem" could apply here.  to help understand and possibly resolve my issues.

    https://ln5.sync.com/dl/875622290/stys9mg3-ky7jseyq-9avds3rb-pdpa6z85

    I don't use change management tools like github. The above link will provide access to a zip file of the current arduino ino file.

    The code automates the operation of a model train layout. I have used the work on this project in a few posting.   Pulse Width Modulation a Speed Equalizer(6): The locomotive has arrived in the final post  I'm Board...Cutting Board to Printed Circuit Board  Two trains labeled Siding and Main are controlled using the code. The goal is to alternately switch the two trains onto a loop of track. First one then the other. The code controls turnout switching, speed management and alternating each train.

    https://ln5.sync.com/dl/ca9b041f0/nge29iak-a4mpe5gi-bnvfxbdd-rwi9ubig

    A short video showing the trains in action can be found at the link.

    lines of code 255-273 & 357-374 are the delay areas I am currently trying to resolve.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to colporteur

    Where did you get the L298NX2 library from? I'd like to see that in more detail.

    FYI, not related to your problem, since I do not think that code is using it, but you have an error with motor_delay.

    int motor_delay = 900000;   //delay for motor to move train

    You cannot store more than 32,767 in a signed variable 16-bit variable. If you want to use 900,000 then you need to make it an unsigned long.

    Also not related to your problem, but I want to bring it up now... the way you are using millis() does not handle roll-over correctly. (Although, that should not be a problem for another 48 days.)

    The problem is that your comparison will (very likely) rollover before millis() does, which is going to result in unexpected logic. The correct way to handle millis() rollover is by using subtraction. When you subtract two unsigned integers, you get the absolute difference between them.

    time_now = millis();
    while (millis() < time_now + turnout_delay)

    Let's just say the rollover event occurs at 1000 for these variable types. Then let's say turnout_delay = 250 and when you assign millis() to time_now, both are (momentarily) 900. The first time that while statement is evaluated, millis() will have incremented 1-2 counts which means your evaluation is: 902 < (900 + 250).

    Do you see the problem? 

    The comparison is NOT: 902 <  1150! Because, remember I said (for this example) the variable type that holds the value rolls over at 1000. (unsigned longs rollover at 4 million something, 1000 is easier to type.) So instead your comparison effectively became:

    902 < abs(1000 - (900 + 250)) or 902 < 150!

    So now, you're going to sit there spinning for a while because millis() has to catch up to the values that already rolled over!

    Instead, you should include millis() in the calculation and use subtraction. So your spinlock should be:

    previous_time = millis();
    while (millis() - previous_time <= turnout_delay);

    I have a longer write-up here (skip to the "why does this work" section) if you want to see other examples of how this rollover happens with real code.

    In the meantime, I think we need to look at that library to see what it is doing. I suspect it is futzing with a register or two.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to baldengineer

    https://github.com/AndreaLombardo/L298N the link for the Arduino module to control two motors.

    I think there is some detritus in my code from failed attempts. The motor delay was my attempt at constructing a void function to create a motor delay. I am more aware now of the unsigned long.

    The missus just put supper on the table. I will check in later. Thanks for the insight.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 3 years ago in reply to baldengineer

    https://github.com/AndreaLombardo/L298N the link for the Arduino module to control two motors.

    I think there is some detritus in my code from failed attempts. The motor delay was my attempt at constructing a void function to create a motor delay. I am more aware now of the unsigned long.

    The missus just put supper on the table. I will check in later. Thanks for the insight.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • baldengineer
    baldengineer over 3 years ago in reply to colporteur

    Understandable on the motor_delay. And I recognize it is one of the reasons why it gets tough to share code. People pick apart the things you already know, or think you know, about.

    However, I cannot tell you how many times I've had someone point out some code I thought was commented (or logic'd out) during my debugging.