Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum When is the function delay() a delay?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 41 replies
  • Subscribers 413 subscribers
  • Views 10571 views
  • Users 0 members are here
  • delay
  • arduino_code
Related

When is the function delay() a delay?

colporteur
colporteur over 3 years ago

else if (MainDepartureState == LOW && MainArrivalState == LOW) {
        if (startupMain == HIGH) {
          // pulse turnout for Main train
          digitalWrite(Main_Turnout, HIGH);
          relayDelay();//<-----1
          digitalWrite(Main_Turnout, LOW);
          if (deBug == HIGH) {
            Serial.println("The Main Turnout Activated");
          }
          // Engage Motor for Main
          motors.setSpeedB(minSpeedB);  // Start Motor for Main
          motors.forwardB();
          PowerMain = LOW;
          startupMain = LOW;
          delay(300000);//<----2
          if (deBug == HIGH) {
            Serial.println("Motor Delay Complete");
          }

According to what I have read “The delay() function allows you to pause the execution of your Arduino code for a specified period.”

Why are the delays I am using not working or the values are so extreme? How can I best accomplish a delay?

I tried using the delay() function at point <----1 in my code and it failed miserably. I wanted to activate a relay by turning it on, waiting for relay to engage (delay(2000), then turn it off. The delay(2000) two seconds didn’t work. I wrote a little relay routine that accomplish what I wanted but why did delay(2000) not give me two seconds?

I am using delay() function at <----2 in the code but the value doesn’t reflect the actual delay. I needed to generate some wait time for the motor to engage and trigger a sensor. My desire was a three second delay(3000) but the delay(300000) was a value that actually worked. That would be 300 seconds yes/no?

I'm a code resurrectionist and not an actual programmer. I will try and muddle through discussions 

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +6
    Based on GL shared insight, I used a different set of PWM pins so as not to muck with the delay() timer. I also took the BE suggestions and used subtraction in the millis routines. I am happy to report…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +5
    //user input variables int turnout_delay = 10000; //delay for relay contacts to engage int motor_delay = 900000; //delay for motor to move train unsigned long time_now = 0; int type cannot store outside…
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur +3
    I think that it helps if one can see names like "TCCR0B" and know inside that it is short for "Timer Control Counter Register" then that should immediately set-off alarm bells in one's head. Gough Lui…
Parents
  • colporteur
    colporteur over 3 years ago

    I am going to put aside my reservation about posting full code and look to the baldengineer's suggestion  I somewhat suspect the old adage: "code snippets rarely contain the problem" could apply here.  to help understand and possibly resolve my issues.

    https://ln5.sync.com/dl/875622290/stys9mg3-ky7jseyq-9avds3rb-pdpa6z85

    I don't use change management tools like github. The above link will provide access to a zip file of the current arduino ino file.

    The code automates the operation of a model train layout. I have used the work on this project in a few posting.   Pulse Width Modulation a Speed Equalizer(6): The locomotive has arrived in the final post  I'm Board...Cutting Board to Printed Circuit Board  Two trains labeled Siding and Main are controlled using the code. The goal is to alternately switch the two trains onto a loop of track. First one then the other. The code controls turnout switching, speed management and alternating each train.

    https://ln5.sync.com/dl/ca9b041f0/nge29iak-a4mpe5gi-bnvfxbdd-rwi9ubig

    A short video showing the trains in action can be found at the link.

    lines of code 255-273 & 357-374 are the delay areas I am currently trying to resolve.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to colporteur

    //user input variables
    int turnout_delay = 10000;  //delay for relay contacts to engage
    int motor_delay = 900000;   //delay for motor to move train
    unsigned long time_now = 0;

    int type cannot store outside of -32,768 to 32767 in AVR-based boards. Suggest you use unsigned long. Variable motor_delay will have the wrong value as far as I can tell due to overflow.

      //increase PWM freq to reduce locomotive motor hum
      TCCR1B = TCCR1B & B11111000 | B00000001;  // pin 12 for PWM frequency of 31372.55 Hz Siding
      TCCR0B = TCCR0B & B11111000 | B00000001;  // pin 13 for PWM frequency of 62500 Hz Main

    This is probably what is breaking delay as this is reconfiguring timers! Timer 0 is needed for delay(), so I'd say the second line (TCCR0B) is breaking it.

    - Gough

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to Gough Lui

    I totally agree with Gough. I misread the register names when I looked at the code. (I thought they were both the same register!)

    Are Serial.print()s working?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 3 years ago in reply to Gough Lui

    Awesome catch, Gough Lui  !

    colporteur , you can probably test this by adding that line into the Blink sketch to see what happens.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to baldengineer

    serial prints appear to be working.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to Gough Lui

    WOW folks blown away with your input.

    I wasn't aware of limitation on variables. I know some of the basic about types but this unsigned long is something I need to be more aware of.

     ntewinkel suggestion to test delay(0 was spot on. loading (TCCR0B) in void setup and LED no blink anymore.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to Gough Lui

    I plan to make some PWM pin changes to hopefully eliminate the problem. I currently use pin 12 & 13. The plan is to use pin 44 & 46

    Code for Available PWM frequency for D44, D45 & D46:

    TCCR5B = TCCR5B & B11111000 | B00000001; // for PWM frequency of 31372.55 Hz

    Can you tell me if this change will cause any possible issues?

    Break....Break...

    What made you aware the void setup conflicted with the delay()

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to colporteur

    delay() relies on micros() which relies on TIMER0.

    You can see the full code here:

    https://github.com/arduino/ArduinoCore-avr/blob/master/cores/arduino/wiring.c

    Jump to line 106 for delay() and then look at micros() right above it.

    Also also, notice how delay() is using milils() (with subtraction!) to do the actual delay time ... (which is similar to what you were trying to do in some sections of your code.)

    delay() isn't magic, it is just a loop.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • baldengineer
    baldengineer over 3 years ago in reply to colporteur

    delay() relies on micros() which relies on TIMER0.

    You can see the full code here:

    https://github.com/arduino/ArduinoCore-avr/blob/master/cores/arduino/wiring.c

    Jump to line 106 for delay() and then look at micros() right above it.

    Also also, notice how delay() is using milils() (with subtraction!) to do the actual delay time ... (which is similar to what you were trying to do in some sections of your code.)

    delay() isn't magic, it is just a loop.