Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Montana Kid's Robotics Club Continuous 2 servo locomotion Is there a way to command the servo to completely stop?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 412 subscribers
  • Views 1395 views
  • Users 0 members are here
Related

Montana Kid's Robotics Club Continuous 2 servo locomotion Is there a way to command the servo to completely stop?

PROFCW
PROFCW over 3 years ago

We are building an IR Arduino uno controlled (from NEC remote)  mobile robot with two servos.  Now we used the usual servo library and it worked well until we tried to stop the servo. The servo will drift ever so slightly, because the servo is updated about every 20 milliseconds, therefore it drifts and the robot at stop continues to move.  Is there a way to command the servo to completely stop?  I thought of a cutoff power rellay but maybe there's a better way

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago +3
    Both ways are good. If you kill the PWM signal (e.g. reconfigure the pin to be an input or set the PWM to an invalid value) then a decent (or semi-decent, or even some very low-end! but not always) hobby…
  • dougw
    dougw over 3 years ago +1
    Servo hunting or drift may be due to several things like load, servo position, coupling stiffness, local vibration, power fluctuations, etc. Hobby servos typically don't have adjustable loop gain or integral…
  • strb
    strb over 3 years ago +1
    Based on your description I understand that after setting the value that should means "no servo rotation" you continue getting a slight rotation, right? If so, you could try to find by trial and error…
Parents
  • robogary
    robogary over 3 years ago

    Tough one. Usually a futaba continuous servo has a teeny tiny zero adjust pot , that's the most obvious thing to try to make it perfect. It still may drift depending on temperature or just in jostling it around.

    Fyi - Zero speed is 1.5 ms pulse width every 20 ms. I'm not sure how the servo library handles multiple servos, could be arduino pwm accuracy, but also could be the servo itself drifting and offset. A mosfet could be put upstream to cut all servo power. I'm not sure what happens if pulse width goes to zero. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 3 years ago

    Tough one. Usually a futaba continuous servo has a teeny tiny zero adjust pot , that's the most obvious thing to try to make it perfect. It still may drift depending on temperature or just in jostling it around.

    Fyi - Zero speed is 1.5 ms pulse width every 20 ms. I'm not sure how the servo library handles multiple servos, could be arduino pwm accuracy, but also could be the servo itself drifting and offset. A mosfet could be put upstream to cut all servo power. I'm not sure what happens if pulse width goes to zero.