Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Displaying time on an Arduino TFT display using a RTC 3231
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 414 subscribers
  • Views 6063 views
  • Users 0 members are here
  • arduino uno
  • tft display
  • learning
  • DS3231 clock module
Related

Displaying time on an Arduino TFT display using a RTC 3231

Adam_A
Adam_A over 3 years ago

Hi, I was recently working on a new project which displayed time from a real time module to a Arduino TFT display using an Arduino UNO as the main board, however I'm still having trouble with it displaying anything on the screen as when I wire everything up and power the Arduino it just displays a white blank screen,

For the wiring I've made this diagram, (all parts in this diagram represent what I have):

image

And for the code I've added this: 
I have double checked that the library's do work with my display. 

#include <Wire.h>
RTC_DS3231 rtc;
char t[32];
#include "Adafruit_GFX.h"
#include "MCUFRIEND_kbv.h"
MCUFRIEND_kbv tft;

#include "Fonts/FreeSans9pt7b.h"
#include "Fonts/FreeSans12pt7b.h"
#include "Fonts/FreeSerif12pt7b.h"
#include "FreeDefaultFonts.h"

#define PI 3.1415926535897932384626433832795
#define WHITE 0xFFFF

int col[8];

void showmsgXY(int x, int y, int sz, const GFXfont *f, const char *msg)
{
  int16_t x1, y1;
  uint16_t wid, ht;


  tft.setFont(f);
  tft.setCursor(x, y);
  tft.setTextColor(0x0000);
  tft.setTextSize(sz);
  tft.print(msg);
}
void setup()
{
  Serial.begin(9600);
  Wire.begin();
  rtc.begin();
  rtc.adjust(DateTime(F(__DATE__),F(__TIME__)));
  //rtc.adjust(DateTime(2019, 1, 21, 5, 0, 0));
   tft.reset();
  uint16_t ID = tft.readID();
  tft.begin(ID);
  tft.setRotation(1);
  tft.invertDisplay(true);
  tft.fillScreen(0xffff);
}
void loop()
{
  DateTime now = rtc.now();
  sprintf(t, "%02d:%02d:%02d %02d/%02d/%02d", now.hour(), now.minute(), now.second(), now.day(), now.month(), now.year());  
  Serial.print(F("Date/Time: "));
  Serial.println(t);
  showmsgXY(170, 250, 2, &FreeSans9pt7b, t);
  delay(1000);
}


I personally think that the issue is with the wiring however again I'm not sure if it is the code or wiring which I'm messing up, as when I wire everything up it just displays a blank screen like this:

image

Final goal target to be displayed on the screen:

image

If anyone has worked with such displays and knows what's the issue any help would be highly apricated, thanks! 


  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 3 years ago in reply to Adam_A +2
    I presume the text libraries only overwrite the character pixels so previous pixels do not get blanked. I always write a blank before the update but it can flicker as the character momemtarily goes blank…
  • Andrew J
    Andrew J over 3 years ago in reply to shabaz +2
    Once you’ve got it working in the simplest, easiest case you could look at getting more complex: only print what changes. The date only changes as midnight; the hour once every 60 mins etc. So print the…
  • javagoza
    javagoza over 3 years ago +1
    There are many such modules. If you can add a reference to the spec sheet or where you bought it they may help you better. I have used several of these modules as in this project Arduino UNO Chess Clock…
Parents
  • dougw
    dougw over 3 years ago

    https://www.youtube.com/watch?v=RG6aejGy3Z0&ab_channel=GadgetReboot

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Adam_A
    Adam_A over 3 years ago in reply to dougw

    Yeah I saw this, I had no issues running these programs however when it came to simply displaying time from a real time module thats where everything got complex
    there is also this video which goes over on how to, when I used his code it actually displayed the digits on my screen however it wasn't syncing with the time model. 
    https://www.youtube.com/watch?v=WhfvWn5oli8&t=169s 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 3 years ago in reply to Adam_A

    When you say it wasn’t syncing with your time model what do you mean? It would help if you could show how it is connected, what your serial debug is showing.  The guy in this video has it plugged directly into a Mega, with a UNO I think you have to wire it - where did you get the info for doing that?  If you have updated code that “sort of works” you could post that.  The fact you say it is now displaying digits seems to imply that it may just be a simple coding error, however you are drip-feeding info to us, rather than giving us the full picture of what you have and what you have tried which makes the conversation a lot longer (and more frustrating on this side)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Andrew J
    Andrew J over 3 years ago in reply to Adam_A

    When you say it wasn’t syncing with your time model what do you mean? It would help if you could show how it is connected, what your serial debug is showing.  The guy in this video has it plugged directly into a Mega, with a UNO I think you have to wire it - where did you get the info for doing that?  If you have updated code that “sort of works” you could post that.  The fact you say it is now displaying digits seems to imply that it may just be a simple coding error, however you are drip-feeding info to us, rather than giving us the full picture of what you have and what you have tried which makes the conversation a lot longer (and more frustrating on this side)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Adam_A
    Adam_A over 3 years ago in reply to Andrew J

    The code in the video I sent was meant for an Arduino Mega thus it didn't work (I had to basically re-wire it to work with an UNO) 
    Anyways the code I have written in the original post does not reflect the one in the video, the one in the video I just mentioned because I tried it and it didn't work.