Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Looking for a small display recommendation
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 31 replies
  • Subscribers 413 subscribers
  • Views 6664 views
  • Users 0 members are here
  • displays
  • model railroad
  • arduino projects
Related

Looking for a small display recommendation

colporteur
colporteur over 3 years ago

Does any member have a recommendation for a small display that is appropriate for scrolling from right to left?

After an hour culling the adafruit website with few returns, I have come to the E14 community hopefully to get a recommendation. I've been asked to build a two signs, one that scrolls "Welcome to Snow Island"  and the other "Thank you for Visiting Snow" Island. The signs will be positioned on top of a bridge on an HO scale model railroad layout.

I had hoped to use a MAX7219 Dot led Matrix MCU 8x32 but it is way to large for the foot print I have to work with. The bridge has a large flat surface about 4X4 inches to hold the sign.

Like any model railroad project cost is a factor. I don't have a big budget. I'm hoping to combine the display with an Nano Arduino to simulate a continuous text scrolling road sign to message visitors.

If your suggestions could contain the source for the part that would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 3 years ago +5
    Thank you for the input folks. Here are two displays I have ordered. If the displays on the left work it should be fairly simple to finish the project. Very little work on my part. The display on the right…
  • colporteur
    colporteur over 3 years ago in reply to colporteur +4
    community.element14.com/.../IMG_5F00_2289.MOV Do I buy or do I build? The S1144 (far left) displays arrived today. After installing the configuration software the display I wanted was working. At $10…
  • shabaz
    shabaz over 3 years ago in reply to beacon_dave +3
    Just saw these, look quite nice, just under 3.7" wide, available in many colors, and very cheap! However they either work for the use-case, or don't, since the behaviour of them is only configurable…
Parents
  • colporteur
    colporteur over 3 years ago

    image

    Thanks for the response folks.

    Some of your offerings I have looked at and others didn't come up on my radar. I need to do some further research under the heading of EASY. I hoping to avoid investing countless hours in the build.

    In my head I have this idea of soldering some sockets to a breadboard to hold a Nano with a few connections to a display. Bang out some code and the message is flowing. I like the idea of building a shroud around the blue display but the 8X8 was what appealed to me in the beginning. I just don't think the screens would be long enough without adding at least six.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • colporteur
    colporteur over 3 years ago

    image

    Thanks for the response folks.

    Some of your offerings I have looked at and others didn't come up on my radar. I need to do some further research under the heading of EASY. I hoping to avoid investing countless hours in the build.

    In my head I have this idea of soldering some sockets to a breadboard to hold a Nano with a few connections to a display. Bang out some code and the message is flowing. I like the idea of building a shroud around the blue display but the 8X8 was what appealed to me in the beginning. I just don't think the screens would be long enough without adding at least six.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • robogary
    robogary over 3 years ago in reply to colporteur

    I also had the thought that a really REALLY cool train marquee would be a persistence of Vision display like amgalbu built for  Santa Tracker , of course scaled down and use 8 normal LEDs packed together rather than programmable LEDs. 

    This is the HARD way  :-)  but for sure would be eye catching.