Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Model Rocket Flight Computer Altitude / Speed update
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 413 subscribers
  • Views 7699 views
  • Users 0 members are here
  • altitude
  • mpu6050
  • bmp280
  • speed-measuring
  • I2C OLED Display
Related

Model Rocket Flight Computer Altitude / Speed update

Frausing
Frausing over 3 years ago

Hi all, I am new to Arduino

I am trying to make an Model Rocket Flight Computer

I Use an Arduino Nano, an BMP280 and MPU6050 to measure Altitude and Speed
It show it on an small I2C OLED Display

It should show the live data on the display for the first 10 minutes
And after 10 minutes it then should show the Max Altitude and the Max Speed.

I can't get the Altitude and Speed to update on the display, it just keep saying 0.00
and of course after the 10 min. it still say 0.00

BMP280, MPU6050, OLED Display
Is conected to:
VCC to 5V on Arduino Nano
GND to GND
SDA to A4
SCL to A5

The LED is on Pin 13

I hope that someone can help me 

#include <Wire.h>
#include <Adafruit_GFX.h>
#include <Adafruit_SSD1306.h>
#include <Adafruit_BMP280.h>
#include <Wire.h>
#include <MPU6050.h>

#define OLED_RESET 4
Adafruit_SSD1306 display(OLED_RESET);

Adafruit_BMP280 bmp;
MPU6050 mpu;

const int ledPin = 13;
float altitude;
float speed;
int maxAltitude = 0;
int maxSpeed = 0;
unsigned long startTime = 0;

void setup() {
  Serial.begin(9600);
  Wire.begin();
  mpu.initialize();
  bmp.begin();
  display.begin(SSD1306_SWITCHCAPVCC, 0x3C);
  display.clearDisplay();
  pinMode(ledPin, OUTPUT);
  digitalWrite(ledPin, HIGH);
  delay(1000);
  digitalWrite(ledPin, HIGH);
  startTime = millis();
}

void loop() {
  unsigned long elapsedTime = millis() - startTime;
  int secondsElapsed = elapsedTime / 1000;

  if (secondsElapsed < 10) { // Display startup message for 10 seconds
    display.clearDisplay();
    display.setCursor(0, 0);
    display.println("0RocketFlightComputer");
    display.display();
  }
  else if (secondsElapsed < 600) { // Display current altitude and speed for first 10 minutes
    int16_t accelY = mpu.getAccelerationY();
    float accel = accelY / 16384.0 * 9.81; // convert to m/s^2
    altitude = bmp.readAltitude(1013.25);
    speed = accel * altitude;

    if (isnan(altitude) || isinf(altitude)) {
      altitude = 0;
    }

    if (isnan(speed) || isinf(speed)) {
      speed = 0;
    }

    display.clearDisplay();
    display.setTextSize(1);
    display.setTextColor(WHITE);
    display.setCursor(0, 0);
    display.println("RocketFlightComputer1");
    display.setCursor(0,10);
    display.print("Altitude: " + String(altitude, 2));
    // display.println(altitude, 2);
    display.setCursor(0,20);
    display.print("Speed: " + String(speed, 2));
    // display.println(speed, 2);
    display.display();
  }
  else { // Display maximum altitude and speed after 10 minutes
    if (altitude > maxAltitude) {
      maxAltitude = altitude;
    }
    if (speed > maxSpeed) {
      maxSpeed = speed;
    }
    display.clearDisplay();
    display.setTextSize(1);
    display.setTextColor(WHITE);
    display.setCursor(0, 0);
    display.println("RocketFlightComputer2");
    display.setCursor(0,10);
    display.println("Max Altitude: " + String(maxAltitude) + " m");
    display.setCursor(0,20);
    display.println("Max Speed: " + String(maxSpeed) + " m/s");
    display.display();
  }
  delay(100);
}


Test setup

image
image

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +4
    Your code never checks if the sensors were initialised correctly anyway - check return values for mpu.initialize() and bmp.begin(). I suspect you have issues with your I2C connectivity - run a I2C scanner…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to phoenixcomm +3
    Vars don't belong in a header file. I advise arduino users to stick to the setup() and loop() mechanisms. It works well and it 'll be easier to get assistance when you use a common approach.
  • Gough Lui
    Gough Lui over 3 years ago in reply to shabaz +2
    I wonder if it's because people who have not configured a name (rather than having just username) get blanked? shabaz - I'll test it with your name and see what happens. Or perhaps there's some more…
Parents
  • shabaz
    shabaz over 3 years ago

    I can't see clearly from the photos, are you running the modules all from 5V? If so, can you check if the MPU6050 module supports 5V operation? I think it might only support 3.3V operation. 

    Anyway, that needs checking via module datasheet etc.

    (Incidentally, most sensors have moved to 3.3V operation these days, and using a 5V Nano makes life more difficult, compared to just moving to 3.3V microcontrollers and 3.3V supported attached devices).

    Also, you should just try to get one sensor working first (physically disconnect the other sensor). 

    Finally, how will this be used? If it is on a model rocket, then who will be able to read the altitude and speed in-flight? Maybe a logging system would be more usable (perhaps even without a display etc, to make it lighter).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago

    I can't see clearly from the photos, are you running the modules all from 5V? If so, can you check if the MPU6050 module supports 5V operation? I think it might only support 3.3V operation. 

    Anyway, that needs checking via module datasheet etc.

    (Incidentally, most sensors have moved to 3.3V operation these days, and using a 5V Nano makes life more difficult, compared to just moving to 3.3V microcontrollers and 3.3V supported attached devices).

    Also, you should just try to get one sensor working first (physically disconnect the other sensor). 

    Finally, how will this be used? If it is on a model rocket, then who will be able to read the altitude and speed in-flight? Maybe a logging system would be more usable (perhaps even without a display etc, to make it lighter).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Frausing
    Frausing over 3 years ago in reply to shabaz

    Hi, Good eye you got :-)

    yes now it is on 5V did first run it on 3.3 V
    and the MPU6050 can run on 3 to 5V

    I have just changed it to 3.3V again, no change

    I did not look at the datasheet, I just found it here: https://components101.com/sensors/mpu6050-module
    Will find the datasheet :-)

    I have just run an example code on each modul, and they say they work.

    This will be on an small 1 meter rocket, I did first try with an SD card reader and it shake sometime too much. So the data is corrupted
    I did read that the copper connections from the SD card reader can do that. thats why I will try this.

    Thats why I have set it up, so the first 10 minutes, it should show the live data, and after 10 min. it then show the MAX.
    Then I can see that it work, before I send. and I can see the Altitude before I send the rocket. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Frausing

    The circuit at that site shows that even if the MPU module is powered with 5V, the I2C lines are pulled up to 3.3V. The BME280 module I think expects 3.3V.

    You really need to check carefully what voltage levels each board expects on the I2C lines, and what power supply each board can be powered from, and then connect it accordingly. If the Nano only has 5V GPIO, then you have an incompatibility there too.

    Best advice: redesign the solution, using a more modern microcontroller, and any modern sensors and display that have 3.3V compatible GPIO.

    Pi Pico springs to mind, it is a similar size to the Arduino Nano, but has more normal (nowadays) 3.3V level GPIO.

    I'm confused about this comment:

    This will be on an small 1 meter rocket... Thats why I have set it up, so the first 10 minutes, it should show the live data

    Who can read the display during the time the rocket is in flight, if that flight time occurs for a period within those ten minutes? If you wish to reduce the size and weight further, then another idea is to remove the display (another benefit is that it is one less device to power up if you don't include it, and one less thing that needs compatible I2C voltage levels). Incidentally the microcontroller in the Nano contains EEPROM, which could be used for storage perhaps. If that's not enough, an external memory chip should be soldered.