Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum circuit connexion of potentiometer and external speaker
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 44 replies
  • Subscribers 412 subscribers
  • Views 8740 views
  • Users 0 members are here
Related

circuit connexion of potentiometer and external speaker

naimlion
naimlion over 3 years ago

hi please i want to change the sound volume using potentiometer and a speaker with arduino.can you help me to do the connection circuit .thx in advance 

kind regards

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 3 years ago in reply to naimlion +3
    Hi, There's just two or three wires on the potentiometer. I strongly suggest you just wire it up (in any way you think fit, you can google this), and see what happens. You'll learn more from that experience…
  • JWx
    JWx over 3 years ago in reply to phoenixcomm +2
    In the end it turned out that it was software task - potentiometer was supposed to drive software based volume control, which the author finally achieved...
  • shabaz
    shabaz over 3 years ago in reply to naimlion +1
    Hi, You're not bothering me, this is genuinely the best advice I can think of. It's the best way to learn, just to try it, because in this particular instance, you're very unlikely to damage anything…
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    You just cant pick a random pot. The problem you have is called impedance. You need to know what the impedance of the speaker is. 4, 8, 16 ohms This part is an L-pad,  Where the L-pads resistance has to match the speakers. There are also T-pads, Basically, the pad keeps the impedance constant value. so in an L-pad, there are two pots wired together like the letter L, so while one pot goes up the other goes down. if you want a more detailed explanation go to the wiki

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • phoenixcomm
    phoenixcomm over 3 years ago

    You just cant pick a random pot. The problem you have is called impedance. You need to know what the impedance of the speaker is. 4, 8, 16 ohms This part is an L-pad,  Where the L-pads resistance has to match the speakers. There are also T-pads, Basically, the pad keeps the impedance constant value. so in an L-pad, there are two pots wired together like the letter L, so while one pot goes up the other goes down. if you want a more detailed explanation go to the wiki

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • naimlion
    naimlion over 3 years ago in reply to phoenixcomm

    so if it´s difficult to use this speaker ok no problem forget it .can we use microbit speaker and potentiometer to change sound volume

    regards

    • Cancel
    • Vote Up -1 Vote Down
    • Sign in to reply
    • Cancel
  • naimlion
    naimlion over 3 years ago in reply to naimlion

    here my code in makecode

    makecode.microbit.org/_iPWXs1d3o0v4

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • naimlion
    naimlion over 3 years ago in reply to naimlion

    we can also  use an other speaker with 2 pins only :gnd to gnd of microbit and the other pin to p1 for exp and i desactivate the microbit speaker and all works well.

    the issue appears when i want to use potentiometer to change sound volume  that´s it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • naimlion
    naimlion over 3 years ago in reply to phoenixcomm

    please pin NC in my speaker do you know what??

    because i don´t use it but when i worked without potentiometer and i don´t connect this pin all works well and i  listen music

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 3 years ago in reply to phoenixcomm

    it has turned out that this is not a "speaker" but LM386 module with speaker (and builtin pot for volume regulation)...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • naimlion
    naimlion over 3 years ago in reply to JWx

    so i change sound volume only with this blue knob ?i can´t change sound volume with my personal potentiometer connected to microbit?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to JWx

    Then this Arduino schematics will help

    AKX00037-schematics.pdf (arduino.cc)

    from Arduino Make Your UNO Kit — Arduino Online Shop

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • JWx
    JWx over 3 years ago in reply to naimlion

    You can - simply add another potentiometer at the input :)