Arduino
  • Products
  • More
Arduino
Arduino Forum Rate my arduino code
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 411 subscribers
  • Views 5759 views
  • Users 0 members are here
Related

Rate my arduino code

scottiebabe
scottiebabe over 3 years ago

I have never used an actual arduino board and have only tried the arduino framework on non-arduino hardware a few times.

I am putting together a little test box for an ADS1115 ADC module (or clone of  New clone on the block  ) 

Quite stuff inside the box, noisy stuff outside the diecast box, nothing fancy.

image

I am using a RPI Pico running the arduino framework using platformio

image

Here is the code I put together using Adafruits arduino library for the ADS1115

// Sample an ADS1115 ADC via i2c with a RPI Pico
// PICO GPIO20 - I2C_SDA
// PICO GPIO21 - I2C_SCL
// PICO GPIO16 - ADS1115_DRDY
//
// Inspired by Adafruit demo, use as you like.
// scottiebabe/sstobbe@2n3904blog.com

#include <Wire.h>
#include <Adafruit_ADS1X15.h>

// GPIO16 ISR
void ADSInterrupt();

Adafruit_ADS1115 ads1115;
MbedI2C i2c(20,21);  // Use GPIO Pins 20,21 on Pico for i2c

void setup(void)
{
  Serial.begin(9600);
  //while (!Serial);
  delay(1000);
  Serial.println("Hello!");
  Serial.println("Getting single-ended readings from AIN0..3");
  Serial.println("ADC Range: +/- 6.144V (1 bit = 187.5uV)");
  ads1115.begin(0x48,&i2c);

  // Enable Pico's onboard LED
  pinMode(LED_BUILTIN, OUTPUT);
  digitalWrite(LED_BUILTIN,1);

  // Setup ISR on GPIO16
  pinMode(16,INPUT_PULLUP);
  attachInterrupt(16, ADSInterrupt, FALLING );
  gpio_pull_up(16);

  Serial.println("Hello, pt2!");
  Serial.println("Configured ADS1115 for single channel continuous conversion.");
  Serial.println("ADC Range: +/- 256mV (1 bit = 7.8125 uV)");
  Serial.println("Fs: 860 Sa/s");
  Serial.println("Ain: Ain0-single ended");
  //ads1115.setGain(GAIN_TWOTHIRDS); // SET FSR +-6V
  ads1115.setGain(GAIN_SIXTEEN); // Set FSR +- 256 mV
  ads1115.setDataRate(RATE_ADS1115_860SPS);
  //ads1115.startADCReading(ADS1X15_REG_CONFIG_MUX_DIFF_0_1,true);
  Serial.println("Starting Acquisition! ...");
  ads1115.startADCReading(ADS1X15_REG_CONFIG_MUX_SINGLE_0,true);
}

#define ADS_BUF_LEN (4096)
volatile int16_t  samples[ADS_BUF_LEN] = {0};
volatile uint32_t tstamps[ADS_BUF_LEN] = {0};
volatile int adsidx = 0;
volatile int adsinterrupt = 0;

// GPIO16 ISR
void ADSInterrupt() {
  if( adsidx < ADS_BUF_LEN ){
    tstamps[adsidx] = time_us_32();
  }
  adsinterrupt = 1;
}

/* Adafruit Demo Loop
void loop(void)
{
  int16_t adc0, adc1, adc2, adc3;

  adc0 = ads1115.readADC_SingleEnded(0);
  adc1 = ads1115.readADC_SingleEnded(1);
  adc2 = ads1115.readADC_SingleEnded(2);
  adc3 = ads1115.readADC_SingleEnded(3);
  Serial.print("AIN0: "); Serial.println(adc0);
  Serial.print("AIN1: "); Serial.println(adc1);
  Serial.print("AIN2: "); Serial.println(adc2);
  Serial.print("AIN3: "); Serial.println(adc3);
  Serial.println(" ");
  
  delay(1000);
}
*/

void loop(void){

  if(adsinterrupt){
    if( adsidx < ADS_BUF_LEN ){
      samples[adsidx] = ads1115.getLastConversionResults();
      adsidx++;
    }
    adsinterrupt = 0;
  }

  if(adsidx >= ADS_BUF_LEN){
    //Print out the sample buffer to serial console
    Serial.println("Acquisition Buffer:");
    for(int i=0; i<ADS_BUF_LEN; i++){
      Serial.print(tstamps[i]);
      Serial.print(",");
      Serial.println(ads1115.computeVolts(samples[i]),7);
      delay(1);
    }

    
    // dummy read to re-arm interrupt
    ads1115.getLastConversionResults();
    adsidx = 0;
    adsinterrupt = 0;
    Serial.println("Starting Acquisition! ...");
  }
}

Thumbsup / Thumbsdown

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +4
    I'd move the defines and global variables to the begin, under the includes. That's the only nitpick.
  • kmikemoo
    kmikemoo over 3 years ago +3
    Not that this will help any at all but... if it runs, it's always a .
  • scottiebabe
    scottiebabe over 3 years ago in reply to Jan Cumps +3
    Using this decorator puts my function in sram
Parents
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    Serial.begin(9600);

    I never had issues even with Uno R3, running the serial terminal at 115200 baud.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    Serial.begin(9600);

    I never had issues even with Uno R3, running the serial terminal at 115200 baud.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • scottiebabe
    scottiebabe over 3 years ago in reply to wolfgangfriedrich

    I wasn't really sure about that, I am using the USB port on the pico for serial communication. I just copied what I saw in an adafruit example, I don't know if it actually gets used with USB CDC.