Arduino
  • Products
  • More
Arduino
Arduino Forum Custom i2c with Arduino UNO.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 411 subscribers
  • Views 1937 views
  • Users 0 members are here
  • ports
  • i2c
  • programming
  • uno
  • pinout
  • arduino
Related

Custom i2c with Arduino UNO.

A_N_T_O_N
A_N_T_O_N over 2 years ago

For educational purposes, I would like to write my own i2c protocol. Is it possible to write a custom i2c library to communicate using regular ports, or should I use the SCL and SDA ports? Do the SCL/SDA ports have special hardware implementations, or can you configure any port for i2c?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 2 years ago +1
    SCL/SDA are open drain outputs. (SDA can also be an input) If a digital pin can be configured as an open drain output, possibly with an internal pull-up resistor, it can be used for a custom I2C implementation…
  • beacon_dave
    beacon_dave over 2 years ago +1
    A_N_T_O_N said: Do the SCL/SDA ports have special hardware implementations The microcontroller datasheet is useful for that sort of information.
  • dougw
    dougw over 2 years ago +1
    You could use any digital output as an open drain output if you add a FET to the output, but it is tricky to use the same pin for input.
Parents
  • javagoza
    javagoza over 2 years ago

    The answer is yes and not. If the Arduino acts as master and you don't need multiple masters or high speed the answer is yes.

    There are several libraries you can use as inspiration as this one GitHub - stevemarple/SoftWire: Software I2C implementation for Arduino and other Wiring-type environments

    Another option could be using three pins and a tristate buffer like the SN74HC125 data sheet, product information and support | TI.com but if you only need to implement the master side, it can be feasible only using pinMode(), digitalWrite() and digitalRead() functions.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 2 years ago

    The answer is yes and not. If the Arduino acts as master and you don't need multiple masters or high speed the answer is yes.

    There are several libraries you can use as inspiration as this one GitHub - stevemarple/SoftWire: Software I2C implementation for Arduino and other Wiring-type environments

    Another option could be using three pins and a tristate buffer like the SN74HC125 data sheet, product information and support | TI.com but if you only need to implement the master side, it can be feasible only using pinMode(), digitalWrite() and digitalRead() functions.