Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Multiple servo control...setting expectations
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 409 subscribers
  • Views 6215 views
  • Users 0 members are here
  • arduino_code
  • code
  • servo_motor_control
Related

Multiple servo control...setting expectations

colporteur
colporteur over 2 years ago

image

Can six servos all operate independent using and Arduino and PCA9685 PWM driver?

I am creating an model railroad barn yard animation scene. Six different animal perform movements using SG90 servos.

The cows in ellipse A tails moves left to right.

The cow in ellipse B moves its head left to right

The cow in ellipse C moves its head up and down

The pig in ellipse D moves it head up and down

The pig in ellipse E moves its head from left to right.

The modeller has asked that all animals perform motion at the same time. Cow tails swing. Cow heads move and pigs heads move. Each animal would complete a pattern. i.e. Cow C dips it head to gather feed and then raises it head to chew. 

I'm confident I can create the servo action to simulate the motion individually. I'm not so sure if this is possible simultaneously.

I stuck on the concept of a thread. If the cows tails are moving that has to stop for the other animals to move.

Can some Arduino aficionados provide me some guidance? Is it possible to do this all with one Arduino or does it have to be broken down to be done by one or more Arduino?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 2 years ago +11
    community.element14.com/.../IMG_5F00_2571.MOV Here is a short video using the code shabaz provided. I made a few tweaks in array values to get the desired effect.
  • shabaz
    shabaz over 2 years ago +7
    Hi Sean, It can certainly be done with a single Arduino as mentioned by others, but it takes a different code structure than just the basic loop. The luxury method would be to use a real-time operating…
  • michaelkellett
    michaelkellett over 2 years ago in reply to colporteur +6
    Slightly scary - I keep expecting one to take its first step ! MK
Parents
  • colporteur
    colporteur over 2 years ago

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Here is a short video using the code shabaz provided. I made a few tweaks in array values to get the desired effect.

    • Cancel
    • Vote Up +11 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to colporteur

    That's fantastic! The animations really work for the animals. And when there is general ambient sound from attendees or background music etc., the servo noises will not be noticeable. Presumably the noises are heard more by the mic because the camera is on that board. The servo noise is lower I guess for listeners, since the servos are on the underside.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 2 years ago in reply to colporteur

    That's fantastic! The animations really work for the animals. And when there is general ambient sound from attendees or background music etc., the servo noises will not be noticeable. Presumably the noises are heard more by the mic because the camera is on that board. The servo noise is lower I guess for listeners, since the servos are on the underside.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • colporteur
    colporteur over 2 years ago in reply to shabaz

    The farm yard scene is very rough at the moment. The modelers will do the cosmetic stuff. There is a fence around the area, additional static animals, feed troughs and painting to cover glue and create wear areas.

    I have used a better quality servo to reduce the noise. At shows with the floor noise it won't be an issue.

    Much thanks to you for the code. I'm rather embarrassed to take credit. My wife keeps thinking I'm smart. I try and tell her I just know really smart people.

    I will post a final video when it is complete and installed.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to colporteur

    Glad you tried it out! I wasn't sure how it would go. Nice to see all the hard work with the mechanics work well in this case with the code+timings!