Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Multiple servo control...setting expectations
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 409 subscribers
  • Views 6215 views
  • Users 0 members are here
  • arduino_code
  • code
  • servo_motor_control
Related

Multiple servo control...setting expectations

colporteur
colporteur over 2 years ago

image

Can six servos all operate independent using and Arduino and PCA9685 PWM driver?

I am creating an model railroad barn yard animation scene. Six different animal perform movements using SG90 servos.

The cows in ellipse A tails moves left to right.

The cow in ellipse B moves its head left to right

The cow in ellipse C moves its head up and down

The pig in ellipse D moves it head up and down

The pig in ellipse E moves its head from left to right.

The modeller has asked that all animals perform motion at the same time. Cow tails swing. Cow heads move and pigs heads move. Each animal would complete a pattern. i.e. Cow C dips it head to gather feed and then raises it head to chew. 

I'm confident I can create the servo action to simulate the motion individually. I'm not so sure if this is possible simultaneously.

I stuck on the concept of a thread. If the cows tails are moving that has to stop for the other animals to move.

Can some Arduino aficionados provide me some guidance? Is it possible to do this all with one Arduino or does it have to be broken down to be done by one or more Arduino?

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 2 years ago +11
    community.element14.com/.../IMG_5F00_2571.MOV Here is a short video using the code shabaz provided. I made a few tweaks in array values to get the desired effect.
  • shabaz
    shabaz over 2 years ago +7
    Hi Sean, It can certainly be done with a single Arduino as mentioned by others, but it takes a different code structure than just the basic loop. The luxury method would be to use a real-time operating…
  • michaelkellett
    michaelkellett over 2 years ago in reply to colporteur +6
    Slightly scary - I keep expecting one to take its first step ! MK
Parents
  • colporteur
    colporteur over 2 years ago

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    Here is a short video using the code shabaz provided. I made a few tweaks in array values to get the desired effect.

    • Cancel
    • Vote Up +11 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago in reply to colporteur

    Slightly scary - I keep expecting one to take its first step !

    Slight smile

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to michaelkellett

    I'm trying to figure out a way to do have an animal walk. The HO scale moulded animals don't have a lot of plastic to work with. The moment so far is done by hacking up two animals to create joints to connect parts for one animal to move.

    I hope to add barn yard sounds to this display to mask some of the servo noise.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to colporteur
    colporteur said:
    I'm trying to figure out a way to do have an animal walk.

    Perhaps you need to rear some Strandbeest on your farm.

    https://en.m.wikipedia.org/wiki/File:Strandbeest-Animation-rgb-100ms.gif

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 2 years ago in reply to colporteur

    There is a rather cool thing called magnorail which I have seen with tiny animated bicycles. Might be able to do something with walking animals?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to colporteur

    It sounds like you've just added scope - to create barnyard sounds that coincide with the servo sounds. AT least you already have trigger code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to dougw

    I think this could be feasible with a Pi Pico.

    I'm thinking that if each animal sound was stored as a WAV, then a Pi Pico could mix in each animal sound as it is triggered. The Arduino code could be modified to store trigger times as part of the animation sequence perhaps, and send that to Pi Pico. That would be a nice 2-microcontroller solution. It would be attractive to do it this way because any number of animal sounds could be made simultaneously, as long as there's enough storage for the sounds. 2 seconds of sound for each animal, at 24ksps, would use up half a Mbyte for 6 animals, so would comfortably fit in a Pi Pico. If there were (say) two or more cows, then that would only count as one animal but it could be played for all cows simultaneously at either different times, or even partially overlapping times. Even slight frequency changes for animals of the same type could be possible as a stretch goal! But that's harder..

    There is example code for a sinewave here, which could be perhaps adapted: https://github.com/raspberrypi/pico-playground/blob/master/audio/sine_wave/sine_wave.c

    Stretch goal #2: Stereo, allowing a parameter that specifies where the animal is on the board, so that the sound can be positioned approximately. It's all building up to a major project with the stretch goals though.. maybe could be used as a commercial sound fx module for exhibitions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to beacon_dave

    BD you always bring something to the conversation that is neat! I don't think I can fit the mechanics in the white cow. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to shabaz

    I would love to work at the Model Railroad layout in Germany where you could actually play with this stuff for a living. I would have to share my salary with you, you did write the code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 2 years ago in reply to shabaz

    My thought is a JQ6500 with a few mp3 files. I have to learn very little to accomplish that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to Workshopshed

    Nice. The Magnorail setup uses a clear disc against the road surface as a drive wheel for animating the legs.  

    image

    With two discs, you get four leg drive...

    image

    Perhaps add a drive belt to keep them in sync though otherwise it could be 'Ministry of Silly Walks' time.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 2 years ago in reply to Workshopshed

    Nice. The Magnorail setup uses a clear disc against the road surface as a drive wheel for animating the legs.  

    image

    With two discs, you get four leg drive...

    image

    Perhaps add a drive belt to keep them in sync though otherwise it could be 'Ministry of Silly Walks' time.

    • Cancel
    • Vote Up +3 Vote Down