Arduino
  • Products
  • More
Arduino
Arduino Forum Servo Movement At Power Up Before Initialization
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 411 subscribers
  • Views 3814 views
  • Users 0 members are here
  • servo
  • arduino
Related

Servo Movement At Power Up Before Initialization

colporteur
colporteur over 2 years ago

I am experiencing a problem with the servos operations on this project that members helped me develop.

When the Mega is powered on the servo track to a position before going to the initialized position. The power on position for the servo is outside the range of motion for the animation. The movement has over extended some mechanical connections and caused breakage.

I went in search of a solution and found this post. It doesn't solve the problem but the discussion is an example of what I am experiencing. One of the suggestions is to relay control power. Only apply power to the servo after full initialization thereby avoiding the issue.

I'm curious if anyone has experienced a servo movement issue on power up and how they may have solved it.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +3
    Hi Sean, The power on position is really the position with no PWM applied. I can think of four potential solutions. (a) Ideally there would be a mechanical solution (i.e. as Frank mentions, to try…
  • colporteur
    colporteur over 2 years ago in reply to beacon_dave +3
    I successfully adjusted the physical connection on one servo today after determining "horn initialization position" I was fortunate since the horn works from 90 to 0. 90 being the start and the initialization…
  • genebren
    genebren over 2 years ago in reply to colporteur +3
    Hi Sean, I build a series of DMX driven decoders that come in 6 and 12 servo channels. These boards have a switchable power bus that provides up to 10 Amps of servo power. On power up, the servo power…
Parents
  • colporteur
    0 colporteur over 2 years ago

    My environment has me working with multiple servos and multiple arduino's mainly Nano and Mega. I'm not confident I have all the knowledge regarding what I am calling "Power on servo initialization position". The scenario is a servo connected to an Arduino moves to a specific position when power is applied and then moves to the coded position when under control.

    I have worked with a number of SG90, SG92 &  MG90S Micro Servo motors over the years and I have had anomalies happen that I couldn't explain. At first I thought it was something I imagined since I couldn't duplicate it. The more I work with the servos the more I can't ignore the anomalies. I would like to find out why.

    How is the power on initialization positions determined?

    What causes a servo initialization position to change?

    Will the power on initialization positions change if I change the Arduino?

    I've installed servo and had them working to having them not align later. I realign the mechanics, then to have them move again sometime back to their original position. I've immediately switched the servo thinking it is at fault. The same scenario has happened with different servos. It is frustrating to say the least.

    I'm going to grab a few servo's and a few different arduinos and run some tests to gather some data in the hope of developing a better understanding. If anyone has any insight to share, I welcome the contribution.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • genebren
    0 genebren over 2 years ago in reply to colporteur

    Hi Sean,

    I build a series of DMX driven decoders that come in 6 and 12 servo channels.  These boards have a switchable power bus that provides up to 10 Amps of servo power.  On power up, the servo power is off until the servo pulses are started.  In addition, the boards use EEPROM memory to store multiple parameters for each of the servos, like Min, Max and Default values to provide a sane range for each servo and to have then start at default value.  On startup the current position variable (RAM) is set to the default value, which can be updated with incoming commands to change this position.

    A neat thing about the switchable servo power is that you can also use this feature for servo position update timeouts, so that the boards do not always drive the servos.  Also, on my boards, I measure the current flow on the servo power bus and shut it off if the current exceeds a programmable level (this has saved my client big bucks as he uses expensive and powerful servos).

    Let me know if you need any more information.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • genebren
    0 genebren over 2 years ago in reply to colporteur

    Hi Sean,

    I build a series of DMX driven decoders that come in 6 and 12 servo channels.  These boards have a switchable power bus that provides up to 10 Amps of servo power.  On power up, the servo power is off until the servo pulses are started.  In addition, the boards use EEPROM memory to store multiple parameters for each of the servos, like Min, Max and Default values to provide a sane range for each servo and to have then start at default value.  On startup the current position variable (RAM) is set to the default value, which can be updated with incoming commands to change this position.

    A neat thing about the switchable servo power is that you can also use this feature for servo position update timeouts, so that the boards do not always drive the servos.  Also, on my boards, I measure the current flow on the servo power bus and shut it off if the current exceeds a programmable level (this has saved my client big bucks as he uses expensive and powerful servos).

    Let me know if you need any more information.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • colporteur
    0 colporteur over 2 years ago in reply to genebren

    The project is small and doesn't have either the financial or physical commitment to take a commercial route. I take on maker projects and soon become disillusioned because they never include the fine print that identifies the pit falls a person is likely to encounter.