Arduino
  • Products & Partners
  • More
Arduino
Arduino Forum Trying to hook up a DRV8428E stepper motor controller. pls assist.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 410 subscribers
  • Views 1651 views
  • Users 0 members are here
  • stepper_motor
  • motor control
  • wiring
  • Datasheet
Related

Trying to hook up a DRV8428E stepper motor controller. pls assist.

SensoredHacker0
SensoredHacker0 over 2 years ago

Im trying to build a motor control circuit with DRV8428E with some friiends.
I read the datasheet, but the guys got me nervous, They are 4 professional engineers, and they have smoked a bunch of these chips,  I don't want to be the next guy to do it. 
luckily,  they're all out of parts for right now. Even so, I would like to try and ensure my success, when more parts do arrive.

The data sheet has an example of the P version as a stepper motor driver, (I'll be using "DRV8428E")
But across the datasheet, there seems to be some subtle differences, which I find confusing.
https://www.ti.com/lit/ds/symlink/drv8428e.pdf

The chip driving this device will be an esp32. I think AEN, BEN, and nSleep should all get tied high to the 3.3V.
I am also confused about what VRef resistors I should choose for rs1, rs2, and if i should use the layout shown on page 29 of the datasheet.




There doesn't seem to be many projects using this device as a stepper motor control. If anyone has some pointers for me, I would greatly appreciate it.
image

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 2 years ago +3
    When you need info on a TI ic that has little examples in the community, the best source is TI's e2e forum. If you don't find examples by googling, chances are low that anyone on this forum has experience…
  • michaelkellett
    michaelkellett over 2 years ago in reply to SensoredHacker0 +3
    I know it can be a PITA but sometimes it's just the way things are. Because the chip (for whatever reason) is not popular it's going to be much harder to find help. My usual reaction to using a chip…
  • michaelkellett
    michaelkellett over 2 years ago in reply to shabaz +2
    For some reason I can't reply to the OP but can here ! I checked on Aliexpress, hundreds of stepper motor driver modules and boards, none using the DRV8428E. The OP might want to wonder why this is and…
Parents
  • SensoredHacker0
    SensoredHacker0 over 2 years ago

    Recently Confirmed, there is errors on the datasheet. Also, when the motor driver gets reset, it remembers the state even if powered on / off. you have to tie VREF a/b high to reset the state to enable the driver again. also the VREF is tied to dvdd, there was conflicting info on that. the calculation is temperamental, even a slight variation, by 0.1V may make the device extremely likely to trip. TI engineers have confirmed these issues, and hopefully will make appropriate changes to the data sheet soon.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • SensoredHacker0
    SensoredHacker0 over 2 years ago

    Recently Confirmed, there is errors on the datasheet. Also, when the motor driver gets reset, it remembers the state even if powered on / off. you have to tie VREF a/b high to reset the state to enable the driver again. also the VREF is tied to dvdd, there was conflicting info on that. the calculation is temperamental, even a slight variation, by 0.1V may make the device extremely likely to trip. TI engineers have confirmed these issues, and hopefully will make appropriate changes to the data sheet soon.