Arduino
  • Products
  • More
Arduino
Arduino Forum Need help building a jet turbine sound module.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 1 answer
  • Subscribers 409 subscribers
  • Views 4141 views
  • Users 0 members are here
Related

Need help building a jet turbine sound module.

akashthakur0305
akashthakur0305 over 2 years ago

Hi All,
I've been trying to make a Jet engine sound module,
I want to 3d print a turbine model and have a potentiometer control the turbine startup/ spooling up/ spooling down / shutdown sound.
Can't seem to find any Arduino code for playing these sounds.
Either on the board or on a MP3 module.

youtu.be/xpAWZPsR82E

I found a old video on YouTube, no tutorials though,
Can anyone help.


Thanks in advance.

  • Sign in to reply
  • Cancel

Top Replies

  • colporteur
    colporteur over 2 years ago +3
    JQ6500 MP3 Player the sequel I use a JQ6500 sound module with my Arduino projects for sound. You can load the JQ6500 with up to 2M of mp3 and play them individually. The module can be used standalone…
  • rsc
    rsc over 2 years ago +2
    Do a search for RC jet engine sound module and you'll find several devices that you can operate using a PWM channel from the arduino.
  • phoenixcomm
    phoenixcomm over 2 years ago +2 suggested
    akashthakur0305 Ok, I bite, first a sound file is sort of universal. I was a crew chief in the USAF, and when you started you thing it sounded terrible. I suggest, that you don't mess about and print the…
Parents
  • fskrzycki
    0 fskrzycki over 2 years ago

    The sound in this clip is from a turboshaft helicopter engine. You can hear the blades at 1:39.

    The video leaves a lot of questions.  

    Do you want audio to play with a rc transmission radio? Will this speaker be on the plane?

    Side note, it may be cheeper to buy a jet engine than invest the time and money into programming arduino. 

    If you want to create a program that outputs power level depending on the throttle position, I would start with breaking up a engine start up into segments, power changing segments, increase and decrease. Than have separate power level sounds based on the appropriate power level. 

    I would also have to create a sub routine that recognizes the current throttle position and relative direction.  Your going to have a hard time with it not sounding choppy. Aka. The video is most likely fake. 

    Good luck. Let me know how you do. Very interesting challenge for sure. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • akashthakur0305
    0 akashthakur0305 over 2 years ago in reply to fskrzycki

    Hi,

    This is not for a RC plane,

    Im 3d printing a turbojet engine model which I can keep on my desktop,

    Printing the file is easy, making a motor run the turbine with a potentiometer is also figured out,

    But it would be cool if there was background noise of the engine starting up and spooling up along with the turning turbine,

    Controlled with the same potentiometer.

    There are RC engine simulators with esp32 and Arduino, but I can't sleep to modify them for my use, plus they are a little complicated as people have integrated turn signals,headlights and stuff.

    Regards 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fskrzycki
    0 fskrzycki over 2 years ago in reply to akashthakur0305

    If all you want is the turbine spinning why not use a simple circuit with a small electric engine? You can connect the potentiometer to the power supply. I don't see the need to even use a program.. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fskrzycki
    0 fskrzycki over 2 years ago in reply to akashthakur0305

    If all you want is the turbine spinning why not use a simple circuit with a small electric engine? You can connect the potentiometer to the power supply. I don't see the need to even use a program..