Arduino
  • Products
  • More
Arduino
Arduino Forum Arduino IDE 2.3.3 hangs when trying to download boards package_index.json
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Arduino to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 403 subscribers
  • Views 5530 views
  • Users 0 members are here
  • arduino ide
  • serial monitor interaction
  • package_index.json download
Related

Arduino IDE 2.3.3 hangs when trying to download boards package_index.json

ralphjy
ralphjy over 1 year ago

I just ran into an unexpected issue when I was trying to update code for a project.  When I had previously closed the IDE yesterday I had the Serial Monitor open.  Today when I opened the code in a fresh instance of the IDE it got stuck trying to download the first package_index.json that I have in my Additional Boards Manager URLs.

I discovered that it is possibly a known issue with the IDE - Exceptionally long duration of "Downloading index: ....  What fixed it for me was closing the Serial Monitor and reopening it after the IDE finished startup.  I am using IDE version 2.3.3 and there isn't any released update available so I guess the problem is not fixed yet.

Just thought I'd mention it here as it surprised me because I hadn't updated either the code or IDE and would never have expected an interaction with the Serial Monitor.  Maybe I'll just remember to close it when I shutdown.

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 1 year ago +1
    I've been experiencing the same problem for the past two weeks working with Espressif boards, the only solution that works for me is reinstalling the ESP32 board package. I've already read about closing…
  • ralphjy
    ralphjy over 1 year ago in reply to javagoza +1
    I don't update the IDE that frequently so I don't know when this issue started (it appears that it might have been 2.3.x). I'm glad that the workaround didn't require downgrading the IDE version. I have…
Parents
  • javagoza
    javagoza over 1 year ago

    I've been experiencing the same problem for the past two weeks working with Espressif boards, the only solution that works for me is reinstalling the ESP32 board package. I've already read about closing the Serial Monitor, but it won't let me even close it.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 1 year ago

    I've been experiencing the same problem for the past two weeks working with Espressif boards, the only solution that works for me is reinstalling the ESP32 board package. I've already read about closing the Serial Monitor, but it won't let me even close it.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ralphjy
    ralphjy over 1 year ago in reply to javagoza

    I don't update the IDE that frequently so I don't know when this issue started (it appears that it might have been 2.3.x).  I'm glad that the workaround didn't require downgrading the IDE version.  I have noticed that recently when I update the Boards Manager that some of the more active board packages take forever to update.

    The problem does not seem to be boards specific for me - just hangs on the first additional package index it tries to download.  In my case it is the m5stack.  I'm working with a PicoW.

    image

    Too bad you can't just close the Serial Monitor when it hangs.  Just makes it a slight annoyance for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 1 year ago in reply to ralphjy

    I don't usually update it that often either, but I was sent a Waveshare ESP32-S3 2.8inch Capacitive Touch Display Development Board to test and the computer I had on hand didn't have the Arduino IDE installed.

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview